This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High impedance inputs of I/O pins in MSP430



Hi to all,

I am working with Evaluation Module incorporates an intelligent peripheral,
which is controlled via SPI by onboard MSP430 processor.

Sometimes I need to keep the MSPs I/O pins inactive (to make all I/Os are high.impedance inputs) awhile,
and manage onboard peripheral via program SPI by other means.

Could I do this using low level Reset pin on MSP430?
If it' possible, how long could I keep a low level Reset?

Thanks in advance!

Alexei

**Attention** This is a public forum