I have had nothing but problems with the MSP430 Gang Programmer for this application. I have it wired to 8 different boards. Positions 4 & 5 work reliably, and position 5 works 80% of the time, the others continually through Error 27 and Error 25. Thinking it was a board issue I tested 8 separate boards on positions 4 and 5 to confirm they are able to program correctly and then placed them through positions 1-8, the issues continued.
MSP430F5438A
Supplied by Programmer
Voltage 3.3 V
Max 30 mA
JTAG (Fast) - All speeds have been tried