Part Number: MSP430FR2355
Other Parts Discussed in Thread: MSP-FET
Good afternoon,
I run into this error when attempting to program the FR2355 device.
"MSP430: Error connecting to the target: The Debug Interface to the device has been secured"
I have looked into the map file and see no Password set.
I need to re-program this device. It is the first time for me. However, it was programmed by a previous employee.
I am currently using CCS version:
Version: 10.1.1.00004
I have attempted to slow down the debug clock from the xcml file. It did not work.
I am using the MSP Flash Emulator to program the device.
Would you please help in getting access to the device?
I do have the source code and with your direction I can identify information that I might have failed to recognize.
Thanks again and best regards,
Ziggy