This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507:The comparator's reference DAC is used to output a sine wave.

Part Number: MSPM0G3507

I am considering two sine wave outputs, one at 4 kHz and one at 40 kHz.
The 40 kHz sine wave uses DAC12 and DMA.
Therefore, we would like to use a comparator reference DAC for the 4kHz.
How can I switch the reference DAC setting with the DMA to output the sine wave?
(I would appreciate it if you could give me some specifics on how to do this.)
How many microseconds is the settling time of the comparator's reference DAC?

**Attention** This is a public forum