Hi all,
I am using a MSP430F2132 for temperature monitoring applications and would like to know the typical accuracy of the ADC10 integrated temperature sensor.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I am using a MSP430F2132 for temperature monitoring applications and would like to know the typical accuracy of the ADC10 integrated temperature sensor.
Hi Max,
I believe, you can find the answer to your question at the MSP430F2132 datasheet, under temperature sensor.
-kel
Hi llmars,
Aside from the unprofessionally rude comment, I did read the datasheet and the family user guide. Go troll elsewhere.
Thanks Markel,
I did review the spec sheet and the family user guide quite a few times. They were not clear as to what the typical accuracy is.
Max Tibbetts said:I did read the datasheet and the family user guide
On page 46 there's table 10-Bit ADC, Temperature Sensor and Built-In VMID. Check "Sensor output voltage" data, it contains information needed to estimate sensor (initial) accuracy. For instance at 0 degree Celsius sensor min/typ/max output is 895/995/1095 mV. For 25 degree Celsius it's 985/1085/1185 - huge overlap with 0 degree numbers. So as you can see without calibration this temperature sensor is useable only to estimate - msp430 core is really hot or really cold :D I would not recommend to use this sensor for any other functions than temperature correction of msp430 peripherals (like ADC).
[edit] I did read datasheet for you. And in result did not change my mind ;)
Hi llmars,
Thank you for that bit of information. However that did not fully answer my question. Specifically speaking, what is the typical accuracy I can get from this IC with calibration?
Also, please be professional and courteous in your future posts. Rude comments are generally not appreciated by other people, especially so among other engineers,
Hi Max,
As you've pointed out, the datasheet gives no information on the tolerance when using the ADC temperature sensor calibration values. This is in stark contrast to the DCO calibration constants, which have their tolerances specified over temperature and/or supply voltage.
Unless you're lucky enough to get a reply from another engineer who has determined the tolerance empirically I think your best bet is to ask TI technical support directly.
Rob
Max Tibbetts said:Specifically speaking, what is the typical accuracy I can get from this IC with calibration?
Unfortunately I don't know. Absence of detailed performance data for tempsensor clearly shows: not recommended for most of the applications, use at your own risk - do calibration and parametrization yourself :) Also consider that msp430 itself have some heating when loaded. Personally I am happy with LM92 - it ispredictable, works out of the box :)
Max Tibbetts said:Also, please be professional and courteous in your future posts.
LOL thank you :) Peace. In return hints for your future posts:
1) don't post twice. if you accidentally do - there's delete option
2) before you ask - check that documentation/datasheet indeed does not contain answer. if unsure, then briefly tell what you supposedly know - so we see that you are NOT ignorant "give me working code NOW" type, that you did your homework before asking.
Well, tolerance over temperature isn't really a meaningful parameter for a temperature sensor :)Robert Cowsill said:As you've pointed out, the datasheet gives no information on the tolerance when using the ADC temperature sensor calibration values. This is in stark contrast to the DCO calibration constants, which have their tolerances specified over temperature and/or supply voltage.
Basically, the temperature coefficient is constant, so voltage changes linearly with temperature.
However, neither offset nor gain are closely specified. But with the information of a constant temperature coeeficient, both values an be determined by a simple two-point calibration. Apply two known temperatures, read the resulting voltages and you can calculate the offset adn the gain very precisely (only limited by ADC resolution, as its offset and gain errors are part of the calibration results, sufficient settling time after exposing the MSP to these temperatures, and precision of the applied temperature.
Of course, the measured temperature is chip die temperature, not ambient temperature, so depending on the packages thermal resistance and the momentary power dissipation, the measured temperature might be higher than ambient.
Some MSPs have factory-determined values for 30°C and 80°C. So the difference between these two values is the gain for 50°C etc. However, due to limited testing time (production cost) these values aren't that precise. But they have a tolerance specified :)
(own calibration gives better results with tolerance towards 0)
Jens-Michael Gross said:Some MSPs have factory-determined values for 30°C and 80°C. So the difference between these two values is the gain for 50°C etc. However, due to limited testing time (production cost) these values aren't that precise. But they have a tolerance specified :)
Where are those tolerances specified? These are the temperature calibration constants I was referring to in my last post, and there's no sign of tolerance specifications for them in the datasheet.
From the 5x family users guide:
1.13.5.3 Temperature Sensor Calibration
The temperature sensor is calibrated using the internal voltage references. Each reference voltage (1.5/2.0/2.5 V) contains a measured value for two temperatures, 30°C±3°C and 85°C ±3°C and are stored in the TLV structure.
Well, with own calibraiton, I'm sure you can do much better :)
Aha! You're right, as usual, Jens-Michael :)
The 2x family user's guide also specifies the calibration tolerance in the TLV section. Interestingly the 2x chips have better specs than the 5x, with a tolerance of ±2°C!
I wonder why these specifications aren't in the datasheets though. Perhaps TI think the temperature sensor tolerance is so bad that they don't want to shout about it, but they do list the VLO drift with temperature and that's woeful!
I guess the factory test takes more timr on the 2x family than on the 5x family (DCO timing constants are not needed for the FLL), so the 2x family take smore time in the climate chamber and the target temperature is reached closer. Th eproblem is not the temperature sensor offset and gain tolerance itself. It is terrible. THe problem is that a precise calibration requires a long tim ein the climate chamber so that the die temperature is really what it is intended to be. For teh values in teh TLV structure, they only guarantee that the die temperature at the tiem of measurement was close to 30°/85° by +-3 or +-2°C. Sicne you need die temperature and not case surface temperatur, you cannot even measure the current temperature. You can only expose the chip to the proper ambient temperature and wait. And waiting costs money.Robert Cowsill said:I wonder why these specifications aren't in the datasheets though. Perhaps TI think the temperature sensor tolerance is so bad that they don't want to shout about it,
This is why I said that doing your own calibration will surely result in a much higher precision.
VLO is just 'something that somehow oscillates'. Its purpose is clearly specified as a clock souce when low power is by far more important than precision. The datasheet info is based on one-time measurements of a lot of MSPs, but not performed at any MSP from actual production (maybe except for occasional quality checks). You cannot compare the two.Robert Cowsill said:but they do list the VLO drift with temperature and that's woeful!
I'm not complaining about the precision (or lack thereof), just wondering why that information is in the user guide rather than the datasheet.
The tolerances for the DCO calibration values are in the datasheet, so it seems logical that the temperature calibration tolerances would be listed there as well.
Because the temperaure tolerance is a result of the general production and test process and not of any device-specific elements. When testing any MSP of this or that family, the device will reach teh destination temperature only with in this or that range. No matter which MSP it is. The longer the whole test takes (which highly depends on family), the closer the device temperature will be to the target temperature.Robert Cowsill said:just wondering why that information is in the user guide rather than the datasheet.
**Attention** This is a public forum