Hallo everybody,
This is a very silly question but i was wondering if the vref+ for ADC can be set to 3.3V or use the Avcc as ref that runs on 3.3V?
I looked in the datasheet and in the ref document (SLAU208) but cant really figure it. The problem is that i have a sensor running on 3.3V (also the MCu runs on 3.3V) but as far as i can tell the ref can not be set higher than 2.5V that would mean i need some extra IC or something to interface them together.
Any tips or feedback would be very helpfull and please bear with me im still a student and (unfortunately) a slow learner.
Thanks in advance,
jeff