Other Parts Discussed in Thread: PCA9515A
Hello,
I am using I2C of an MPS430F5659 (UCB1, 1k pull-up, 4 sensors, 30cm cable) and I've noticed that the SDA and SCL output in this mode are very weak (raise time of about 1us). If I toggle the output in GPIO mode it seems much stronger (raise time 20ns and 5ns with PxDS activated).
As a result, when I touch my PCB with the hand, SCL stays low and I2C doesn't work, when I do the same experiment when in GPIO mode the SCL line can go high without any problems.
Anybody has an explanation or a workaround (beside doing the I2C with bit banging)?
Thanks in advance for your answers and best regards,
Thierry