This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADXL345 - Code works in single step debug mode but not when running freely

Hi,

I am working on communicating with the ADXL345 accelerometer and my code works fine when I single step debug through the program, however when I run it freely it gets stuck in low power mode after a transmit. Here is the code: 

//  Interfacing ADXL345 accelerometer with MSP430G2553 with I2C communication

//

//                                /|\  /|\

//               ADXL345          10k  10k     MSP430G2xx3

//                slave            |    |        master

//             -----------------   |    |  -----------------

//            |                          SDA|<-|---+->|P3.1/UCB0SDA  XIN|-

//            |                 |  |      |                 |

//            |                        |  |      |             XOUT|-

//            |             SCL|<-+----->|P3.2/UCB0SCL     |

//            |                 |         |                 |

//

//  Attribute: Code modified from I2C multiple byte TX/RX Master example by

//  D. Dang

//  Texas Instruments Inc.

//

//  Code Made By :

//  Prof. Ravi Butani

//  Marwadi Education Foundation, Rajkot GUJARAT-INDIA

//  ravi.butani@marwadieducation.edu.in

//

//  Code Released under Creative Commons By-SA  license

//  Visit creativecommons.org/.../deed.en_US  to know more about license

//  Built with CCS Version 5.1.0

//******************************************************************************

#include <msp430.h>

 

#define NUM_BYTES_TX 2                         // How many bytes?

#define NUM_BYTES_RX 6

#define ADXL_345     0x53

int RXByteCtr, RPT_Flag = 0,x1,y1,z1;       // enables repeated start when 1

volatile unsigned char RxBuffer[6];         // Allocate 6 byte of RAM

unsigned char *PRxData;                     // Pointer to RX data

unsigned char TXByteCtr, RX = 0;

unsigned char MSData[3];

 

void Setup_TX(unsigned char);

void Setup_RX(unsigned char);

void Transmit(unsigned char,unsigned char);

void Receive(void);

 

int main(void)

{

  WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT

  P1SEL |= BIT6 + BIT7;                     // Assign I2C pins to USCI_B0

  P1SEL2|= BIT6 + BIT7;                     // Assign I2C pins to USCI_B0

  P1DIR |= BIT0;

 

  // Init sequence for ADXL345

  //Transmit process

    Setup_TX(ADXL_345);

    RPT_Flag = 1;

    Transmit(0x2D,0x00);

    while (UCB0CTL1 & UCTXSTP);             // Ensure stop condition got sent

 

   //Transmit process

     Setup_TX(ADXL_345);

     RPT_Flag = 1;

     Transmit(0x2D,0x10);

     while (UCB0CTL1 & UCTXSTP);             // Ensure stop condition got sent

 

    //Transmit process

      Setup_TX(ADXL_345);

      RPT_Flag = 1;

      Transmit(0x2D,0x08);

      while (UCB0CTL1 & UCTXSTP);             // Ensure stop condition got sent

 

      // Un-comment next block to change range of ADXL345

    /*

       Setup_TX(ADXL_345);

       RPT_Flag = 1;

       Transmit(0x31,0x01);                            // Range Select at add 0x31 write 0x00 for 2g(default)/ 0x01 for 4g/ 0x02 for 8g/ 0x03 for 16g

        while (UCB0CTL1 & UCTXSTP);         // Ensure stop condition got sent

    */

 

  while(1){

 

         //Transmit process

          Setup_TX(ADXL_345);

          RPT_Flag = 1;

          Transmit(0x32,0xFE);                                   // Request Data from ADXL345 in 2g Range 10Bit resolution

          while (UCB0CTL1 & UCTXSTP);             // Ensure stop condition got sent

 

 

  //Receive process

  Setup_RX(ADXL_345);

  Receive();

  while (UCB0CTL1 & UCTXSTP);             // Ensure stop condition got sent

 

  x1 = (((int)RxBuffer[1]) << 8) | RxBuffer[0];

  y1 = (((int)RxBuffer[3]) << 8) | RxBuffer[2];

  z1 = (((int)RxBuffer[5]) << 8) | RxBuffer[4];

 

  // now You have XYZ axis reading in x1,x2,x3 variable....Bingo... you can play with it as you like....

  // Below if sense x and y angle and Red led is on if its more then 45 or less then -45...

  // you can put your own condition here...

   if ((x1 > 128) || (y1 > 128) || (x1 < -128) || (y1 < -128))

         {

                P1OUT |= BIT0; // red led on

         }

 

         else

         {

                P1OUT &= ~BIT0; // red led off

         }

  __delay_cycles(10000);  // sample rate ~100 samples/sec

                                            // you can change by changing delay

  }

}

 

//-------------------------------------------------------------------------------

// The USCI_B0 data ISR is used to move received data from the I2C slave

// to the MSP430 memory. It is structured such that it can be used to receive

// any 2+ number of bytes by pre-loading RXByteCtr with the byte count.

//-------------------------------------------------------------------------------

#pragma vector = USCIAB0TX_VECTOR

__interrupt void USCIAB0TX_ISR(void)

{

  if(RX == 1){                              // Master Recieve?

  RXByteCtr--;                              // Decrement RX byte counter

  if (RXByteCtr)

  {

    *PRxData++ = UCB0RXBUF;                 // Move RX data to address PRxData

  }

  else

  {

    if(RPT_Flag == 0)

        UCB0CTL1 |= UCTXSTP;                // No Repeated Start: stop condition

      if(RPT_Flag == 1){                    // if Repeated Start: do nothing

        RPT_Flag = 0;

      }

    *PRxData = UCB0RXBUF;                   // Move final RX data to PRxData

    __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0

  }}

 

  else{                                     // Master Transmit

      if (TXByteCtr)                        // Check TX byte counter

  {

    UCB0TXBUF = MSData[TXByteCtr];          // Load TX buffer

    TXByteCtr--;                            // Decrement TX byte counter

  }

  else

  {

    if(RPT_Flag == 1){

    RPT_Flag = 0;

    TXByteCtr = NUM_BYTES_TX;                // Load TX byte counter

    __bic_SR_register_on_exit(CPUOFF);

    }

    else{

    UCB0CTL1 |= UCTXSTP;                    // I2C stop condition

    IFG2 &= ~UCB0TXIFG;                     // Clear USCI_B0 TX int flag

    __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0

    }

  }

 }

 

}

 

void Setup_TX(unsigned char Dev_ID){

  _DINT();

  RX = 0;

  IE2 &= ~UCB0RXIE; 

  while (UCB0CTL1 & UCTXSTP);               // Ensure stop condition got sent// Disable RX interrupt

  UCB0CTL1 |= UCSWRST;                      // Enable SW reset

  UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;     // I2C Master, synchronous mode

  UCB0CTL1 = UCSSEL_2 + UCSWRST;            // Use SMCLK, keep SW reset

  UCB0BR0 = 12;                             // fSCL = SMCLK/12 = ~100kHz

  UCB0BR1 = 0;

  UCB0I2CSA = Dev_ID;                         // Slave Address is 048h

  UCB0CTL1 &= ~UCSWRST;                     // Clear SW reset, resume operation

  IE2 |= UCB0TXIE;                          // Enable TX interrupt

}

void Setup_RX(unsigned char Dev_ID){

  _DINT();

  RX = 1;

  IE2 &= ~UCB0TXIE; 

  UCB0CTL1 |= UCSWRST;                      // Enable SW reset

  UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;     // I2C Master, synchronous mode

  UCB0CTL1 = UCSSEL_2 + UCSWRST;            // Use SMCLK, keep SW reset

  UCB0BR0 = 12;                             // fSCL = SMCLK/12 = ~100kHz

  UCB0BR1 = 0;

  UCB0I2CSA = Dev_ID;                       // Slave Address is 048h

  UCB0CTL1 &= ~UCSWRST;                     // Clear SW reset, resume operation

  IE2 |= UCB0RXIE;                          // Enable RX interrupt

}

void Transmit(unsigned char Reg_ADD,unsigned char Reg_DAT){

    MSData[2]= Reg_ADD;

       MSData[1]= Reg_DAT;

    TXByteCtr = NUM_BYTES_TX;                  // Load TX byte counter

    while (UCB0CTL1 & UCTXSTP);             // Ensure stop condition got sent

    UCB0CTL1 |= UCTR + UCTXSTT;             // I2C TX, start condition

    __bis_SR_register(CPUOFF + GIE);        // Enter LPM0 w/ interrupts

}

void Receive(void){

    PRxData = (unsigned char *)RxBuffer;    // Start of RX buffer

    RXByteCtr = NUM_BYTES_RX-1;             // Load RX byte counter

    while (UCB0CTL1 & UCTXSTP);             // Ensure stop condition got sent

    UCB0CTL1 |= UCTXSTT;                    // I2C start condition

    __bis_SR_register(CPUOFF + GIE);        // Enter LPM0 w/ interrupts

}

 

Any explanation as to why this is happening? 

Thanks,

Micah

  • Hello Micah,

    The only place inside of this code where I see an exit from LPM command is inside of the USCIAB0TX ISR, if you are stuck in low power mode after a transmit then this is because either this ISR is never being serviced or a __bic_SR_register_on_exit(CPUOFF); command is never being reached. For that matter I am confused as to why USCIAB0TX ISR is being used for receiving data from the slave device when the USCIAB0RX ISR would appear to be more appropriate. UCB0TXIFG is set when UCB0TXBUF is empty (a byte has been sent) and UCB0RXIFG is set when UCBoRXBUF has received a complete character.

    Regards,
    Ryan
  • Hello Micah,

    Have you been able to resolve your code problem?

    Regards,
    Ryan

**Attention** This is a public forum