This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432 LaunchPad XDS110 Windows XP drivers do not install correctly

Other Parts Discussed in Thread: ENERGIA

I am trying to connect my MSP432 LP to a WIndows XP (32-bit) computer (having given up on using the Mac due to ongoing USB comms connection problems). I have downloaded and installed the driver package as instructed on the Energia website (XDS110_drivers.zip).

The driver installation says it was succesful however when I plug in the LP for the first time, installation of the TI debug probes driver(s) fail. The comm ports drivers install correctly.

During the driver installation these messages are shown:

"Cannot Install the Hardware

There was a problem installing this hardware:

XDS110 (02.02.04.00) with CMSIS-DAP

An error occured during the installation of the device

A service installation section in the INF is invalid"

Following this, in the Windows Device Manager, there are two devices listed as "XDS110 (02.02.04.00) with CMSIS-DAP", under "Texas Instruments Debug Probes", with yellow exclamation marks. Properties for both devices show that the driver is not installed. There are also 2 XDS110 COMM ports that are installed correctly.

I have tried this with two LP's, and two different XP computers and get the same result.

It therefore looks like there is a bug in the driver INF file somewhere.

Can anyone help? Am currently at a production standstill.

 

Scott

**Attention** This is a public forum