Other Parts Discussed in Thread: MSP430F5529
Hi,
I'm using MSP430F5529 launchpad and I need to transfer data to PC via usb cable as fast as possible.
When I was trying to use USCI_A1 (P4.4 & P4.5) UART and BRCLK=SMCLK=20MHz, the max baud rate I can get is 460800 via MSP Application UART1, but in the datasheet, the max baud rate is 1MHz. I tried this link:

to calculate the configuration values but it did't work for 921600 or 1M. So could anyone tell me what are the values of
clockPrescalar, firstModReg, secondModReg and overSampling to get a 1M baud rate from 20M BRCLK?
Thank you.
Regards,
Eric