This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430 launchpad program

Other Parts Discussed in Thread: MSP430G2553

Hello,

I am making my program using msp430g2553 launch pad. In this i have taken input from P2.4 and i want my output from P2.0, P2.1 and P2.2.

In this program i have to generate the pulse of 500ms from input. and my output will be three low pulses from the three pins. Meaning  whenever i connect my oscilloscope probe to 2.4 i can see the pulse. But the program i made it didn't work. when i connect to the oscilloscope it is showing nothing.

when my input pulse is high i will get the three low pulses output.

here is my code, please check it and tell me what is wrong in the code? since it doesn't contains any error.

code:

#include <msp430g2553.h>

#define CPU_F ((double)16000000)
#define delay_us(x) __delay_cycles((long)(CPU_F*(double)x/1000000.0))
#define delay_ms(x) __delay_cycles((long)(CPU_F*(double)x/1000.0))

char C_1, C_2;

void System_Clock_Init( void )
{
    char i;
    _NOP();
    WDTCTL = WDTPW + WDTHOLD;                                                            // Close Watching dog
    delay_ms(50);                                                                                               / / 1MHz
    if( ( CALBC1_16MHZ == 0xff ) || ( CALDCO_16MHZ == 0xff ) )              // FLASH A was cleared!!!
        ((void (*)())RESET_VECTOR)();
    BCSCTL1 = CALBC1_16MHZ;                                                                      //ACLK=32768Hz
    DCOCTL = CALDCO_16MHZ;  //MCLK=DCOCLK=16MHz
    BCSCTL2 = 0x06;//SMCLK=DCOCLK/8=2MHz
    BCSCTL3 = 0x00;                                                                                            / /cap=1pF
    IE1 &= ~OFIE;                                                                                                   / /close crystal error interrupt
    
    do
    {
        IFG1 &= ~OFIFG;     
        for( i = 0; i < 100; i++ )
        {
            _NOP();
        }
    }
    while (IFG1 & OFIFG);   
    
    _NOP();
}

void IO_INIT(void)
{
    NOP();
    P2SEL &= ~BIT4;
    P2SEL2 &= ~BIT4;
    P2REN &= ~BIT4;
    /*P2DIR |= BIT2;*/
    P2IES |= BIT4;
    P2IE  |= BIT4;
    P2IFG  &= ~BIT4;

    P2SEL &= ~(BIT0+BIT1);
    P2SEL2 &= ~(BIT0+BIT1);
    P2REN &= ~(BIT0+BIT1);
    //P2DIR &= ~(BIT0+BIT1);
    P2OUT &= ~(BIT0+BIT1);

    P2SEL &= ~BIT2;
    P2SEL2 &= ~BIT2;
    P2REN &= ~BIT2;
    //P3DIR &= ~BIT1;
    P2OUT &= ~BIT2;
    
   
}

void main(void)
{
    System_Clock_Init();
    _NOP();
    //WDTCTL = WDT_ARST_1000;
    _NOP();      
    IO_INIT();
    _NOP();
    _EINT();//open all interrupt
    _NOP();
    LPM3;
    _NOP();
    while(1);
}

//------------------------------------------------------------------------------
//Function: Start Timer 0 A0 for Hour Timing 500ms
//------------------------------------------------------------------------------
#pragma vector = PORT2_VECTOR
__interrupt void PORT_C_Interrupt(void)

{
 
  _NOP();
  delay_us(20);

  if( C_1 == 0xff)
  {
    if(!( P2IN & BIT4 )) C_2 = 0xff;
  }
  else
  {
      if(!( P2IN & BIT4 )) C_1 = 0xff;
  }
  if(( C_1 == 0xff) && ( C_2 == 0xff))
  {
    //output A B D
    P2OUT |= BIT0;
    delay_ms(2);
    P2OUT |= BIT1;
    P2OUT &= ~BIT0;
    delay_ms(2);
    P2OUT |= BIT2;
    P2OUT &= ~BIT1;
    delay_ms(2);
    P2OUT &= ~BIT2;   
    delay_ms(2);
    
    P2OUT ^= BIT1;                 //P2 toggle
    P2IFG &= ~BIT1;                //IFG cleared 
    C_1 =0x00;
    C_2 =0x00;
  }
  _NOP();
}


**Attention** This is a public forum