Part Number: MSP430G2231
I just need to confirm that it is permitted to have a pullup or pulldown resistor enabled when using P1.1 as the TimerA capture input. So if I begin by using P1.1 as a normal I/O input with a pulldown resistor, then later set the SEL bit high and use the pin as the CCI0A input, the pulldown resistor will remain enabled. Is that correct?
Thanks