Part Number: MSP430FR2311
Hi Team –
Posting on customer behalf.
We are using the MSP430FR2311 16 Bit configuration….
I have a couple of questions about the Clock Frequency calibration and trimming.
1. What is the tolerance on the clock frequency when I am using a 16MHz clock? I see in the users manual that I wouldn’t really be needing a software trim function if I am running within a certain range of frequencies. My understanding is that 16MHz is in that range of frequencies.
2. Do I need to be doing anything on my end for using the factory calibration value? If I set the DCOFTRIMEN to 0 , would that be enough for the clock to use the DCOFTRIM value during factory calibration?
3. I see that the clock is off, and running slow. So, I had to use the Software trim on my demo board for my modules to work right. Any suggestions to minimize the error?
Thank you,
Dan