Part Number: MSP430G2553
Hi I m trying to simulate an interface between msp430g2553 and an OLED display (powered by ssd1306 ) I have attached the code below , can anyone tell me why is it that the port one is set to low even though the PINSEL function sets p1.6 and p1.7 for I2C ?
#include <msp430.h>
/*
0xAE, // Display off
0x81, // set contrast controll register
0x7F, // contrast Wert 127 ok
0x20, // Set Memory Adress Mode
0x01, // Vertical Adressing Mode
0x21, // Set Column Adress
0x00, // Start Adress 0
0x7F, // End Adress 127
0x22, // Set Page Adress
0x00, // Start Adress 0
0x07, // End Adress 7
0x40, // set start line adress 0
0xA0, // Column Adress mapped to SEG0
0xA8, // set multiplex ratio
0x3F, // maximum
0xC0, // Set COM Output Scan Direction to normal mode
0xD3, // set display offset
0x00, // 0
0x8D, // Set Charge Pump Setting
0x14, // ON
0xDA, // set com pins hardware conf
0x12, // alternative + disable remap
0xD5, // set display clock divide + freq
0x80, // divide by 1 and medium freq
0xD9, // set pre charge preriod
0x22, // medium (reset value)
0xDB, // set vcomh
0x20, // 0.77 x Vcc
0xA4, // Output follows RAM Content
0xAF // Display on*/
const unsigned char Init[] = {0xAE,0x81,0x07,0x20,0x01,0x21,0x00,0x7F,0x22,0x00,0x07,0x40,0xA0,0xA8,0x3F,0xC0,0xD3,0x00,0x8D,0x14,0xDA,0x12,0xD5,0x80,0xD9,0x22,0xDB,0x20,0xA6,0xA4,0xAF};
//const unsigned char Init[] = {0xAE,0x81,0x07,0x20,0x01,0x21,0x00,0x7F,0x22,0x00,0x07,0x40,0xA0,0xA8,0x3F,0xD3,0x00,0x8D,0x14,0xD5,0x80,0xD9,0x22,0xDB,0x20,0xA6,0xA4,0xAF};
const unsigned char Mod[] = {0xA5};
unsigned int i = 0;
//unsigned int I = 0;
void printC(const unsigned char* Array, unsigned int length){
UCB0CTL1 = UCSWRST;
UCB0CTL0 = UCMODE_3 + UCMST + UCSYNC; // I2C master mode
UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB0BR0 = 0x40; // < 100 kHz
UCB0I2CSA = 0x3C; // address
UCB0CTL1 &= ~UCSWRST;
IE2 |= UCB0TXIE; // Enable TX ready interrupt
__disable_interrupt();
UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition
__bis_SR_register(LPM3_bits + GIE);
unsigned int c;
for(c = 0; c < length; c++){
//__bis_SR_register(LPM3_bits + GIE);
UCB0TXBUF = 0x80;
__bis_SR_register(LPM3_bits + GIE);
UCB0TXBUF = Array[c];
__bis_SR_register(LPM3_bits + GIE);
}
UCB0CTL1 |= UCTXSTP;
IE2 &= ~UCB0TXIE;
}
void printS(void){
UCB0CTL1 = UCSWRST;
UCB0CTL0 = UCMODE_3 + UCMST + UCSYNC; // I2C master mode
UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB0BR0 = 0x40; // < 100 kHz
UCB0I2CSA = 0x3C; // address
UCB0CTL1 &= ~UCSWRST;
IE2 |= UCB0TXIE; // Enable TX ready interrupt
__disable_interrupt();
UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition
__bis_SR_register(LPM3_bits + GIE);;
}
void printD(const unsigned char Data){
UCB0TXBUF = Data;
__bis_SR_register(LPM3_bits + GIE);
}
void printE(void){
UCB0CTL1 |= UCTR + UCTXSTP;
}
void main(void){
WDTCTL = WDTPW + WDTHOLD;
DCOCTL = CALDCO_8MHZ; //DCO setting = 8MHz
BCSCTL1 = CALBC1_8MHZ; //DCO setting = 8MHz
// Configure Pins for I2C
P1SEL |= BIT6 + BIT7; // Pin init
P1SEL2 |= BIT6 + BIT7; // Pin init
printC(Init,31);
__delay_cycles(8000000);
printC(Mod,1);
/*
printS();
UCB0TXBUF = 0x00;
__bis_SR_register(LPM3_bits + GIE);
unsigned int i;
for(i = 500; i > 0; i--){
printD(0xFF);
printD(0x00);
}
printE();*/
while(1);
}
// USCI_B0 Data ISR
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void){
IFG2 &= ~UCB0TXIFG;
__bic_SR_register_on_exit(LPM3_bits); // Wakeup main code
}