Part Number: MSP430F5659
I am using CCS V6.2 and running the MSP USB descriptor tool, V5_00_11_22, to generate a single CDC virtual COM port for a custom board, MSPF5659, with a USB port. When I install the INF file on Windows 7 (64-bit), SP1 the driver fails to start with Error Code 10. I have attempted to load the driver onto two machines, and have had the same startup failure. If I attempt to update the driver I am told that the driver is up to date.
The Device Manager shows the FET ports as MSP Application UART1 (COM6) and MSP Debug Interface (COM5). The generated CDC port is listed as Virtual COM Port(CDC)(COM11) and has a yellow exclamation since it is not starting.
I would expect the generated driver to load in the registery as a USB Port since it is assigned COM11. However, when I look in HKLM\System\CurrentControlSet\Enum\USB I don't find the device. I have found that the device is being put into \HKLM\System\CurrentControlSet\Enum\Root\Ports\0000. The Device Manager shows the FET ports as enumerated USB devices within the registry.
If I attempt to use the "example" PID of 0x0300 for a single interface CDC and generate an INF file with this address, I receive an error message that the driver is incompatible for x64 based systems. I am attaching the generated INF file which clearly shows a 64-bit section, renamed to .txt.
; --COPYRIGHT--,BSD
; Copyright (c) 2012, Texas Instruments Incorporated
; All rights reserved.
;
; Redistribution and use in source and binary forms, with or without
; modification, are permitted provided that the following conditions
; are met:
;
; * Redistributions of source code must retain the above copyright
; notice, this list of conditions and the following disclaimer.
;
; * Redistributions in binary form must reproduce the above copyright
; notice, this list of conditions and the following disclaimer in the
; documentation and/or other materials provided with the distribution.
;
; * Neither the name of Texas Instruments Incorporated nor the names of
; its contributors may be used to endorse or promote products derived
; from this software without specific prior written permission.
;
; THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 'AS IS'
; AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
; THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
; PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
; CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
; EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
; PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
; WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
; OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
; EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
; --/COPYRIGHT--
; MSP430 Virtual COM Port Installation file for Win2000/XP/Vista/7
;
; Port drivers setup
;
; Supported operating systems:
; Windows 32-bit and 64-bit
[Version]
Signature="$Windows NT$"
; CatalogFile=MSP430_CDC.cat
; For information on CatalogFile, please see
; http://msdn.microsoft.com/en-us/library/windows/hardware/ff547502(v=vs.85).aspx
Class=Ports
ClassGuid={4D36E978-E325-11CE-BFC1-08002BE10318}
Provider=%TI%
DriverVer=09/06/2013, 1.02
[Manufacturer]
%TI%=DeviceList, NTamd64
[DestinationDirs]
FakeModemCopyFileSection=12
DefaultDestDir=12
[SourceDisksNames]
[SourceDisksFiles]
;You can modify next string and place your VID and PID
[DeviceList]
%DESCRIPTION0%=TIUSB, USB\Vid_2047&Pid_0300
[DeviceList.NTamd64]
%DESCRIPTION0%=TIUSB.NTamd64, USB\Vid_2047&Pid_0300
;------------------------------------------------------------------------------
; Windows 32-bit Sections
;------------------------------------------------------------------------------
[TIUSB.nt]
include=mdmcpq.inf
CopyFiles=FakeModemCopyFileSection
AddReg=TIUSB.nt.AddReg
[TIUSB.nt.AddReg]
HKR,,NTMPDriver,,*ntkern
HKR,,NTMPDriver,,usbser.sys
HKR,,EnumPropPages32,,"MsPorts.dll,SerialPortPropPageProvider"
HKR,,PortSubClass,1,01
[TIUSB.nt.Services]
AddService=usbser, 0x00000002, DriverService
[TIUSB.nt.HW]
include=mdmcpq.inf
[DriverService]
DisplayName=%DESCRIPTION%
ServiceType=1
StartType=3
ErrorControl=1
ServiceBinary=%12%\usbser.sys
LoadOrderGroup=Base
;------------------------------------------------------------------------------
; Windows 64-bit Sections
;------------------------------------------------------------------------------
[TIUSB.NTamd64]
include=mdmcpq.inf
CopyFiles=FakeModemCopyFileSection
AddReg=TIUSB.NTamd64.AddReg
[TIUSB.NTamd64.AddReg]
HKR,,NTMPDriver,,*ntkern
HKR,,NTMPDriver,,usbser.sys
HKR,,EnumPropPages32,,"MsPorts.dll,SerialPortPropPageProvider"
HKR,,PortSubClass,1,01
[TIUSB.NTamd64.Services]
AddService=usbser, 0x00000002, DriverService
[TIUSB.NTamd64.HW]
include=mdmcpq.inf
;------------------------------------------------------------------------------
; String Definitions
;------------------------------------------------------------------------------
[Strings]
TI="Texas Instruments"
DESCRIPTION="MSP430-USB Test"
DESCRIPTION0="Virtual COM Port (CDC)"
Any help would be appreciated.
Thanks,
Sean