This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Input mode / Current leakage/ pull up resistor

Part Number: MSP432P401R

Hi , I'm using p4.6 as an input without internal pullup or pull down, the datasheet states that the max current leakage in input mode is 20nA, however after adding an external pullup 50k ohms, there is about ~2uA of current following into the msp432 input pin?..  is my interpretation correct,  there should only be 20nA of current when the pin is set to high impedance mode. Is there ant special states / registers to set ? I would like to use this in an ultra low power application.

Thanks

**Attention** This is a public forum