For my design, I need to use the package quoted in the title, and am looking at the MSP432 hardware design files schematic. I just have a few questions about what blocks are actually required for my design after looking at the datasheets extensively.
Required peripherals:
-5 Digital out pins
-1 ADC input @ 20 kHz+ w/ 12+ bits of accuracy - putting signal through op-amp, so signal level can be changed, and planning on a reference of 2.5 V since it seems that's built in
Questioned block requirements:
1. Do I need the DC-DC block?
2. Do I need the Digital/Analog VCC blocks? If not, do I still have AVCC1/2 connected across a resistor and DVSS1/2/3 and AVSS1/2/3 connected to ground?
3. Do I need the LFX/HFX blocks? I assume not, as 3 MHz processing should be plenty for what I'm doing
4. Is DCOR always connected to the R5 91k resistor into ground?
5. Do I need the RESET block if I don't plan on ever resetting, just power cycling? If not, should I just keep this pin at 3.3 V?
6. Since I plan on using another Launchpad 432 to (no debug) program the PCB 432, the only connections between the 2 I need are:
SWCLKTCK, SWDIOTMS, PJ.5/SWO (SWDIO?), PJ.4/TDI, and RSTN/TMI
into a 10POS connector, correct (of course with the 3.3V source on 1 and 3,5,7,9 all grounded)?