Hello,
I'm currently struggling with the device which is not found by either CCSv4.2.1.00004 nor IAR Kickstart. WinXP Pro. SP2 v2002
http://processors.wiki.ti.com/index.php?title=MSP430_JTAG_Interface_USB_Driver
The MSP FET430 UIF is shown in Windows Hardware Manager as Virtual Com Port. According to this file: http://focus.ti.com/lit/ug/slau278f/slau278f.pdf (Appendix C)
CCS, configured with the target as TI MSP430 USB1/MSP430 [MSP430] (tried all USB and LPT ports...there are no COM ports visible in CCS)
gives me following error:
Error initializing emulator: No USB FET was found (which is the same with no device connected)
IAR Kickstart is producing similar results.
Many people are experiencing this kind of Problem, but it seems to have no simple solution.
What do I need to do to get this running?