I am having difficulties with the MSP430-449STK2 development board and the MSP430-JTAG-Tiny on Windows 7 Ultimate. I am trying to use the Download and Debug the Test Code and I receive the message: "The Fuse Has Been Blown" using the IAR Workbench 5.20.1 (5.20.1.50215). Using the Olimex MSP Programmer I have no problems but I receive a message about "no data loaded in data section" but I can Erase, Verify, Write and Read the device. I installed the JTAG-Tiny and copied the .dll inside BIN folder exactly as described. I figured something out while trying to fix it. When copying the 1.041 drivers and trying to debug I receive the messages I mentioned below. When copying the 1.039 drivers I do not receive the "blown fuse" message, I receive the message attached instead. I do not know how to fix it.