Hello All,
I am looking at implementing an ultra low power/long life embedded DAQ device. I want to take data at a rate of about 4 Bytes/s and then store this to an SD card. The major issue that I am seeing now is that the SD cards can draw upwards of 100 mA during a write operation! This would suck the battery dry very fast.
I was thinking to use a FRAM IC as an external memory buffer. This would allow me to store significant amounts of data, and then write it all to the SD card in one burst for average power savings.
Does anyone have suggestions on how I could best go about this?
Thanks,
Alex