Dear People,
Does anyone have any links, or otherwise usefull information regarding how the MSP430F5XXX can interface the CANopen network.
Regards,
Td.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear People,
Does anyone have any links, or otherwise usefull information regarding how the MSP430F5XXX can interface the CANopen network.
Regards,
Td.
The 430 doesn’t have a CAN protocol controller, you need to get an external CAN controller (note this is in addition to the differential bus transceiver which is always needed). There are some available on the market (not from TI) with SPI but also a parallel-type bus interface (from Philips and others).
For an optimized TI-only solution I would recommend the use of a lower-end TMS470 device or a C2000 device.
There are requirements for an in-vehicle low power solution that neither the TMS470 and C2000 device offer. NOTE to TI marketing. Add a CAN controller to your MSP430. Add functionality to wake up the 430 from sleep on receipt of a can message. You will sell a bunch.
Here is a link to a CAN BoosterPack for the MSP430: http://forum.43oh.com/topic/4202-can-boosterpack/
Does this booster pack actually work with the MSP430F5438A , this is sort of the same setup I have with a CAN controller (MCP2515), CAN transceiver (sn65hvd230).? Do I need an external CAN drivers to actually implement this in my design.
I agree.
Although for those wanting a quick solution it is fairly easy to implement using an external MCP2515.
**Attention** This is a public forum