This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5739 Alarm Setup

Other Parts Discussed in Thread: MSP430FR5739

Hi everyone;

I am trying to get the alarm to work properly on my msp430fr5739 but unfortunately it seems that every time the alarm is supposed to trigger, the processor just ignores it.  I believe that I am setting up the registers incorrectly but I haven't been able to figure out how they need to be configured.  This is the code I'm currently using

void RTC_init(void)
{
RTCCTL01 |= RTCHOLD + RTCRDYIE + RTCAIE;        // hold rtc for setting; enable rtc ready interrupt; 1sec
RTCSEC = 0;
RTCMIN = 0;
RTCHOUR = 0;
RTCAMIN = 1;
RTCAHOUR = 0;
RTCCTL01 &= ~(RTCHOLD + RTCAIFG);                       // release rtchold, begin count
}


// clock init
void CS_init(void)
{
PJSEL0 |= BIT4 + BIT5;                                      // XT1
CSCTL0_H = 0xA5; // Unlock register
CSCTL1 |= DCOFSEL0 + DCOFSEL1;           // Set max. DCO setting
CSCTL2 = SELA_0 + SELS_3 + SELM_3;     // set ACLK = XT1; MCLK = DCO
CSCTL3 = DIVA_0 + DIVS_0 + DIVM_0;         // set all dividers
CSCTL4 |= XT1DRIVE_0;
CSCTL4 &= ~XT1OFF;

do
{
CSCTL5 &= ~XT1OFFG;                    // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
}while (SFRIFG1&OFIFG);                 // Test oscillator fault flag
CSCTL0_H = 0x01;                             // Lock Register
}


// RTC_b isr


#pragma vector=RTC_VECTOR
__interrupt void rtc_isr(void)
{

switch(__even_in_range(RTCIV,0x12))
{
case RTCIV_NONE: break;                           // No interrupt
case RTCIV_RTCRDYIFG:                            // rtc ready
while (!(RTCRDY));
PJOUT ^= BIT0;

sec = RTCSEC;
min = RTCMIN;
hrs = RTCHOUR;

break;

case RTCIV_RTCTEVIFG:               // rtc interval timer

// do nothing here for now

break;

case RTCIV_RTCAIFG:
PJOUT ^= BIT2;
timeToSend = 1;
break;                                                       // rtc user alarm
case RTCIV_RT0PSIFG: break;         // rtc prescaler 0
case RTCIV_RT1PSIFG: break;         // rtc prescaler 1
case RTCIV_RTCOFIFG: break;        // rtc oscillator fault
default: break;

}

}

According to the user's guide, as well as a few examples I've sen I need to use the AE (alarm enable bit) for the respective alarm registers.  However, AE does not exist in the msp430fr5739.h file.  Most of the set-ups that I have seen for similar micro-controllers look something like this

RTCAMIN = AE | (timer & 0x7F);

with "timer" being the value at which you want to trigger the alarm interrupt.  

Does anyone know if there is an equivalent AE bit in the msp430fr5739.h file? or am I doing something else incorrectly that anyone can point out?

Please tell me what I am missing here, or any advice that you think would be helpful

Thanks

Greg

  • Dear Greg:

       I'm not sure if you've solved the problem.

      I met the same thing with you.o(╯□╰)o

      I've found that in the msp430fr5339.h the alarm register's minute and hour are exchanged in AIR's register. I tried to set them as IAR's order, i failed either.

      So, if you've solved the problem, please give me a hand.

      Thank you.  O(∩_∩)O

  • Gregory Wells said:
    RTCAMIN = AE | (timer & 0x7F);


    RTCAMIN really only contains the minute of the alarm. Either as binary value (0x00..0x3b) or in BCD form (0x00..0x59), depending on RTC configuration.

    So a simple &0x7f is surely not sufficient. Except if running the RTC in counter mode.

    If AE is indeed msising in the header file, then you can simply generate it with

    #define AE 0x80

    I guess it has been intentionally been excluded because a global system-wide define of a two-letter toekn isn't a good idea. Maybe there is an RTC_AE define or something like that.

  • RTCAMIN = AE | (timer & 0x7F);
     
    use this as well
  • it works , thanks!

  • Hello Vincent ZHOU (and others too!) 

             I have posted my issues at the end of the thread titled as below:

    "MSP430 example code for Real-Time Clock with Calendar and Alarm functions"

    Can you all please have a look at that post and give some inputs as to what is wrong with my simple code there!

    I'm trying to configure RTC_B of Exp_FR 5739 to generate alarm 4 sec later using ACLK(sourced from VLOCLK).

    Just want to generate some interrupts. Exact time not important.

    Thanks in advance.

    Regards

    Alex

  • Hi ,

    If possible provide us full working code.

    Mine is not working

    -Karthik

**Attention** This is a public forum