Other Parts Discussed in Thread: MSP430G2553
Hello,
For my project I'm planning to use an External Digital Clock of 32768Hz to run the ACKL of the MSP430G2553. The reason is because another component needs also to be clocked at the same frequency. So my idea is to enter the signal to XIN of the MCP430 and connect the XOUT to the other's component XIN.
I know I have to set LFXT1Sx=11 to choose the external clock but I'm not sure about the connection between the MSP430 and the other component. Is it correct my idea?
About the external digital clock, the datasheet says this about the current consumption:
"The current consumption when the output clock is enabled (CLKEN pin at VDD) is a function of the load capacitance on the CLKOUT pin, the output frequency fOUT = 32768Hz and the supply voltage VDD."
Which is going to be the load capacitance seen by the CLKOUT pin when connected to the MSP430? Said in another way, which is the input capacitance in the XIN pin of the MSP430?
Here you can see the Clock datasheet: http://www.emmicroelectronic.com/webfiles/product/other/EM7604_C7_DS.pdf
Thanks
Oriol