Other Parts Discussed in Thread: MSP430F5419A, MSP430F5342
Hi,
Being new to the MPS430 arena I need a basic question answered: “how does one determine if the selected MSP430 chip has shared JTAG pins.”
I see that most all the pins are shared with a general port I/O pin but I do not think that is what is meant by shared pins. I’m trying to enable the BSL on the MSP430F5419A and not sure what pins to connect to. The TI documented pin names do not match the BSL dongle supplier pin names.
The pins on the MSP430F5419A I have selected are:
Pin Name RS232
91 Test RTS
96 RST DTR
18 BSL transmit RXD
19 BSL receive TXD
Can anyone confirm I have selected the correct pins?
And also clarify if the MSP430F5419A has dedicated JTAG pins or not. Per figure 1-2 and 1-3 of the SLA319C manual the RTS line is inverted depending if the MSP430 has shared or dedicated JTAG pins.
Thanks
Gerry