I am using IAR full 5.40.3 MSP430 and CC430F5137. Code compiles without any warning and after trying to flash device I got following error: "A fatal error has occurred. Verify error at address 0cFFF7 on target 0x80 in file 0x84".
I have programmed several identical devices with the same code and no changes has been made. Error appeared after last night WIndows 7 64bit blue screen where it complained something about USB driver. I tried to remove and reinstall IAR but no luck. Any idea?
By default programmer is connected to USB2 port but trying with another USB3 port did not help either.