Hi,
i just try to install the Chronos Access Point (BM-USBD5). When i installed the newest version Chronos-setup.exe everything work well, but after plug-in the access point no driver can be installed. The device manager shows an error for eZ430-ChronosAP. I also changed the the usb_cdc-driver_cc1111.inf file in the Driver-Folder, like someone explained in the TI-forum http://e2e.ti.com/support/microcontrollers/msp430/f/166/t/31051.aspx?pi73932=2, but without any solution. I also copy the file usbser.sys in the %windir%\system32 folder. I also tested the installation on Windows 7 SP1 and on a Windows XP SP2, but both pcs show the same problem. The same problem exist for the debugger device (MSP430 UART).