Other Parts Discussed in Thread: MSP430F1222, MSP430F1232
Here is my configuration:
1.Latest Code composer 5.3.0.00090
2. MPS-FET430UIF
3. My board with msp430F1222
A very simple program: (only to illustrate problem, not work at all)
#include <msp430.h>
/*
* main.c
*/
int main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
return 0;
}
#pragma vector = PORT2_VECTOR
__interrupt void port_vect(void)
{
while(1);
}
When try to upload on the target board and debugging, the error message appear. If change #pragma_vector to something else (PORT1_VECTOR, NMI_VECTOR and so) - no problems.
I check lnk_msp430f1222.cmd and all include files and can't see any strange.The processor type is correct in configuration. This error occurs only if I try to use PORT2_VECTOR !?