Hi,
We have some issues with using the latest MSP-GANG.
I coudn't find more details about BOOT loader and API firmware in the MSP-GANG manual.
Could you please let me know what is the difference between BOOT loader and API firmware commands?
We are trying to control MSP-GANG via firmware commands through RS-232.
The Synchronization Sequence-0x0D works fine and also the Get Progress Status (0xA5) command is successful.
But, when we try to start programming cycle with "send the Main Process Command"
as shown below, the MSP-GANG is returning NACK (0xA0).
Tx-->3e 31 04 04 00 00 00 00 3a 35
The check-sum "3a 35" is calculated as per the Manual.
Please let me know what could be the reason MSP-GANG is returning NACK?
Is there any mistake with the check-sum calculation in the above command.
Regards.
Prad