Other Parts Discussed in Thread: MSP430F5438A
Hi,
Our customer needs to measure a 4-20 mA current signal using an ADC port of MSP430F5438A.
Using 100ohm resistors, the voltage need to convert is going to be 0-2V in theory.
But in practice, because of resistor tolerances and the 4-20mA transmitter at the other
can output slightly more than 20mA at full scale.
We have to make sure that any surge in the current doesnt affect the microntroller
or the interface circuit.
It seems our customer has already burnt few MSP's to this test this application.
We would know
1) Is it ok to use MSP's ADC directly to measure the 4-20mA Current(through 0-2V voltage)
(In this case will it be necessary to add a current-limiting resistor,
which may influence the sampling time of the MSP430 ADC?)
2) or else use additional 4-20mA Current Loop Receiver before the MSP430's ADC?
We would like to know what could be the best solution to measure the
4-20mA current signal through an ADC port of MSP430.
Best Regards.
Prad