Greetings,
I am running Linux Mint 13 (based on Ubuntu 12.04) as a host with Windows XP Pro running within VirtualBox 4.3.2.
I installed CCS v5.5 into VM WinXP only to discover CCS could not detect the FET430 Launchpad interface. I found that I could not set up the the MSP-FET430UIF USB interface link under Devices>USB Devices. It rejected the link attempt and provided the following error message:
>>>>>>>>>>>>>>>
Failed to attach the USB device Texas Instruments MSP-FET430UIF [0105] to the virtual machine WinXPpro.
Failed to create a proxy device for the USB device. (Error: VERR_READ_ERROR).
Result Code:
NS_ERROR_FAILURE (0x80004005)
Component:
Console
Interface:
IConsole {8ab7c520-2442-4b66-8d74-4ff1e195d2b6}
>>>>>>>>>>>>>>>
After spending quite a bit of time with this issue I finally read a VirtualBox forum message that mentioned there is a problem with Linux being overwhelmed during the Linux USB port driver setup from temperature data reports being sent from the MSP430 default application. Removal of the RXD/TXD u-links on the LaunchPad board blocks this data stream and allows one to establish the VB USB Devices link.
My program now runs in the debugger OK. I am pleased as I didn't wish to have the need to dual boot my PC back into Windows just for MSP430 code development.
Hope this tip for a simple work around is helpful!
TMA