This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guys.
I have a Launchpad board and a couple of MSP430 MCUs with me. But the board stopped working entirely. So I want to know if the chips can be programmed without the board. It would be very helpful if that was possible with minimum amount of requirements.
I have a Arduino Uno. I know they both have entirely different MCUs but still will it be possible to make use of the Arduino to program the TI's MCUs ????
Please help me with this guys.
Umm... guys,
sorry. but I am very new to embedded systems, so I don't understand any of the above. can u explain in simple terms or give links to circuit connections and other related stuff... maybe videos and such medias.
my Launchpad is not detected by the energia software on my mac but the power LED is ON and the last uploaded sketch -- red light Blink -- keeps on running all the time. the only problem is that I cant upload new sketches to the chip any longer.
any way to find and rectify the problem is also welcome. :D
thanks for the answers anyways. :)
Bharath Srinivasan said:can u explain in simple terms
The other way to program an MSP is through a JTAG connection. While the BSL is a program that runs on the MSP, JTAG directly controls the CPU from outside. You need a JTAG programmer for this, like the MSP-FET430UIF.
Since it controls the CPU, it can not only write to the MSp memory, but can also be used to debug the running code.
The LaunchPad has a stripped-down FET built-in, so that's the usual way of programming the 2553.
Thank you very much for your answer.
I am planning on trying out the first method.
Can you help by providing a link to the circuit connection along with the list of components required ???
It would be very helpful. Please provide a link to a complete circuit connection diagram, along with any other important points required in the construction of the circuit.
Thank again. :D :D :D :D
Ask Google for MSP430 BSL schematic, and pick one that you like and that is working (software / hardware) on your OS without problems. USB / RS232 3.3V (USB-UART bridge) boards that can work with MSP430 BSL can be found on eBay for few $.
I don't like original TI BSL hardware schematic, and also don't like original TI software side, so I made my own version, that you can see here...
http://e2e.ti.com/support/microcontrollers/msp430/f/166/p/263479/921408.aspx
Complete hardware was packed inside DB9 connector.
Bharath Srinivasan said:sorry. but I am very new to embedded systems, so I don't understand any of the above.
Then better give-up with idea and get LaunchPad :) You will flash your code into microcontroller and it will not work as expected - then what? It's not worth to even try BSL approach and suffer in frustrations - if you are so much beginner. LaunchPad is dirt-cheap. Get it.
Ilmars said:Then better give-up with idea and get LaunchPad :) if you are so much beginner. LaunchPad is dirt-cheap. Get it.
I know that I am a beginner. And that is exactly why I am trying to learn new stuff. Just because I am new to this doesn't mean that I can try a different method.
Just because something is easy and cheap isn't a reason that we must do it and not try other possible solutions.
I want to learn how to program an MSP without using a Launchpad. If you are willing to teach, thank you very much. If not at least don't keep on discouraging people. I know how to buy a new board and connect an USB wire an click the mouse. But that isn't what I want to do. Okay ????
If you know how to do it and wanna help, then HELP. But I don't want you posting any more of your "It can't be done" posts.
Bye.
Bharath Srinivasan said:If you know how to do it and wanna help, then HELP.
Sure! Here it is: http://www.ti.com/lit/pdf/slau319
Also check solution offered by zrno.
Bharath Srinivasan said:I know that I am a beginner. And that is exactly why I am trying to learn new stuff. Just because I am new to this doesn't mean that I can try a different method.
Just because something is easy and cheap isn't a reason that we must do it and not try other possible solutions.
I want to learn how to program an MSP without using a Launchpad. If you are willing to teach, thank you very much. If not at least don't keep on discouraging people. I know how to buy a new board and connect an USB wire an click the mouse. But that isn't what I want to do. Okay ????
If you know how to do it and wanna help, then HELP. But I don't want you posting any more of your "It can't be done" posts.
It can be done on 2 ways, using BSL and/or using JTAG (full 4-wire mode, or 2-wire SBW). I done both, based on my own hardware, and for software starting point used open source TI projects:
slau319 MSP430 Programming Via the Bootstrap Loader (BSL)
slau320 MSP430 Programming Via the JTAG Interface
Already posted link to my BSL version, and my SBW+ multi-prgramer topic is here:
http://forum.43oh.com/topic/2972-sbw-msp430f550x-based-programmer
If you want to learn how to flash MSP430 and have plenty of free time, there is no problem at all. slau319 and slau320 have all you need.
Also, now, original source code for TI FET products is available...
http://processors.wiki.ti.com/index.php/MSPDS_Open_Source_Package
**Attention** This is a public forum