Hello,
We've started to use MSP430F6779 with IAR EW430, and I am trying to enter debug mode.
The board is powered up using an external Vcc, and I am using Spy-Bi-Wire interface, and a MSP-FET430UIF debugger.
I manage to program the chip with an external utility, so I assume this configuration is sufficient(interface, programmer, cable, Vcc).
When I try to enter debug mode from IAR, I get the following error:
Using license: Standalone license - IAR Embedded Workbench for Texas Instruments MSP430 5.60
Firmware version 30301004
Interface dll version 3.3.1.4
Unknown device : (OpenDevice) , Device=MSP430F6779, PwLength=0x0
Fatal error: Could not find device (or device not supported)
Session aborted!
Please advise.
Thanks,
Lior.