Other Parts Discussed in Thread: MSP430F5529
Hi!
What is the better attitude in case I have both XT1 and XT2 populated on the PCB (in this case MSP430F5529 LaunchPad) - use the XT2 crystal (4MHz) as clock signal (XT2CLK) for MCLK or to stabilize the DCO via FLL and use the DCOCLK for MCLK? In my application I do not care much about processing speed therefore I can use 4MHz, I can see these two options presented below - which will be better (the device is going to operate in the field with temperatures changing along the year from -30 to +40 deg of Celsius).
With Regards,
tml