Other Parts Discussed in Thread: MSP430F5659, MSP430WARE, MSP430F6659
I am using your USB firmware upgrade tool version 1.3.0 together with a MSP430F5659 to make firmware upgrades using the BSL.
Whenever the size of the new firmware is equal or bigger then the previous one that is on the MSP430, the firmware upgrade works fine. If I am loading a new firmware that has a smaller size, I always run into a "memory verification error" with that usb firmware upgrade tool. Is there any problem or bug in the verification part of this sample tool?
Just for additional information, I set the correct BSL password in the firmware upgrade tool, and it works fine. So there is no mass erase anymore before loading the new firmware. It must be like this, because for example the bank 3 of the code memory is used for user data that must be available also after a firmware upgrade.
Thanks for your help.