If I'm understanding this correctly, 47k/2.2nF should work for both normal reset operation and spy bi wire mode. IOWs there is no need to change capacitors when moving from normal operating mode to programming mode using spy bi wire.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If I'm understanding this correctly, 47k/2.2nF should work for both normal reset operation and spy bi wire mode. IOWs there is no need to change capacitors when moving from normal operating mode to programming mode using spy bi wire.
Actually, neither part is needed for SBW programming. When doing SBW, the RST pin is controlled by the FETs PUSH/PULL output. But any capacitance will affect the SBW signal timing and prevent SBW access if too large.
However, for ensuring proper startup on power-on (without FET attached), a large R/C time constant (Tau) on RST is required. The slower VCC rises, the larger Tau should be, so RST stays below VCC until VCC has settled.
The two uses contradict: 2.2nF is a value that will be sufficient for most cases while not blocking SBW. But in some cases, 2.2nF isn't enough. In this case you may put a series resistor between the R/C and RST while SBW goes directly to RST. This will reduce the influence of C on SBW while still providing a sufficient Tau. 1k should be enough to use 100nF without influencing SBW.
**Attention** This is a public forum