This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Button Debouncing Code Doubt

Hi,

I'm trying to figure out the debounce routine in this code and I'm also trying to modify it so the sensor will also immediately send a message when the button goes from 0->1. It only sends a message (immediately) when the button goes from 1->0.

The sensor sends messages at every 5 seconds 

I'm pretty new to embedded system and I'm at a loss reagding this button routine.

I would appreciate any help.

Sincerely,

Larissa Eglem.

#include <intrinsics.h>
#include "io430.h"
#include "config.h"

void main(void)
{
//stop watchdog
WDTCTL = WDTPW + WDTHOLD;

//Initiates DCO
clockInit();

//Initiate peripherals
btInitIO();
serialInit();

//Initiates watchdog
WDT_FEED;


__enable_interrupt();
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start

while(1)
{

__bis_SR_register(CPUOFF + GIE); // LPM0 with interrupts enabled

if (tempReady)
{
tempReady = 0;

__no_operation(); // SET BREAKPOINT HERE

ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
}
}
}

/*! \brief sentor tx pins configuration */
static void serialInitIO(void)
{
//IO
TX_PSEL &= ~TX_BIT;
TX_PSEL &= ~TX_PULL;

//hilgh level output
TX_PDIR |= TX_BIT;
TX_HIGH;

//low level output
TX_PDIR |= TX_PULL;
TX_POUT |= TX_PULL;
}

/*button pin configuration */
static void btInitIO(void)
{
// GPIO and input
BT_PSEL &= ~BT_BIT;
BT_PDIR &= ~BT_BIT;
}

Now, here is the interruption:

// Timer A0 interrupt service routine
#pragma vector=TIMER0_A0_VECTOR
__interrupt void Timer_A (void)
{
WDT_FEED;

switch(dbSt)
{
case 0:
if(BT_PIN & BT_BIT)
{
dbCount++;
if(dbCount >= DB_LIMIT)
{
dbTxOffPending = 1; //need to send message with zeros
sensorVal = 0; //value of sensor (0 - button disconnected)
dbSt = 1;
}
}
else
{
dbCount = 0;
sensorVal = 1;
}
break;

case 1:
if(!(BT_PIN & BT_BIT))
{
dbCount++;
if(dbCount >= DB_LIMIT)
{
dbSt = 0;
sensorVal = 1;
}
}
else
{
dbCount = 0;
sensorVal = 0;
}
break;
}

  • The timer ISR checks the state of the button pin on each interrupt. If the button is pressed, a counter is incremented. If the button is released, the counter is reset. If a certain count is reached the button is considered pressed and an action takes place.
    So the button is considered pressed (and debounced) if it stays pressed for DB_LIMIT contiguous interrupts.

     This is a very simple, while effective way to debounce a button if you have the timer running anyways or do not care for low power operation. If you don’t need the timer all the time, then a combination of port pin interrupt and fixed timer delay will allow the CPU to stay in low power mode much longer.
    I have an always-active 1ms timer tick in my application, and I use a similar approach for detecting button presses as well as ‘S0-Bus’ signals (which are also often bouncing due to relay contacts)

  •  "I'm also trying to modify it so the sensor will also immediately send a message when the button goes from 0->1. It only sends a message (immediately) when the button goes from 1->0."

    From what is given,a flag "dbTxOffPending" is set on a 1->0 transition. So you may need to set that flag for 0->1 transition also, I am guessing here (since the message sending routine is not shown) some routine is looking for that flag to be set to send button message and then clear the flag.

    if(dbCount >= DB_LIMIT)
    {
     dbTxOffPending = 1; // Add
     dbSt = 0;
     sensorVal = 1;
    }


    What you could also do in your background loop is to compare sensor states and send a message, since the timer interrupt routines already debounced it.

    if (lastState != newState)
    {
      lastState =newState;
      SendButtonState();
    }
    

     

  • Hi J Joson,

    Thank you for your insights.!

    The problem is that the dbTxOffPending flag is not being cleared in any other part of the code (at least I couldn't see it). Also, the sending routine does not use it.

    Please find attached the entire routine. Your first suggestion, I had previously tried, but had no success.

    I really appreciate your assistence.

    Sincerely,

    Larissa.

    PS: I didn't quite understand the TX_HIGH and TX_LOW bit either. Please, forgive my ignorance. 

    #include <intrinsics.h>
    #include "io430.h"
    #include "config.h"
    
    #define TIPO_ANALOGICO      0x02
    
    // calibracao do sensor de temperatura
    #define CAL_ADC_15T85         (*(unsigned int *)0x10e4)
    #define CAL_ADC_15T30         (*(unsigned int *)0x10e2)
    #define CAL_ADC_15VREF_FACTOR (*(unsigned int *)0x10e0)
    #define CAL_ADC_OFFSET        (*(unsigned int *)0x10de)
    #define CAL_ADC_GAIN_FACTOR   (*(unsigned int *)0x10dc)
    
    //Define a porta de comunica��o e seu bit
    #define TX_PSEL P1SEL
    #define TX_PDIR P1DIR
    #define TX_POUT P1OUT
    #define TX_BIT BIT2
    #define TX_PULL BIT1
    
    //Portas de comunica��o e bit do bot�o
    #define BT_PSEL P1SEL
    #define BT_PDIR P1DIR
    #define BT_PIN P1IN
    #define BT_BIT BIT6
    
    /*! \brief Taxa do oscilador */
    #define CLK 1000000
    
    /*!  \brief Taxa de transmiss�o dos dados */
    #define BAUD 1200
    
    /*!  |brief Numero de ciclos ate que ocorra uma interrup��o de timer */
    #define TIMER_CNTR CLK/BAUD
    
    /*! \brief N�mero de ciclos do debounce */
    #define DB_LIMIT  10
    
    //Estados da m�quina de transmiss�o
    #define START_BIT   0
    #define SEND_DATA   1
    #define SEND_CHK    2
    #define STOP_BIT    3
    #define TX_WAIT     4
    #define RESYNC_HIGH 5
    #define RESYNC_LOW  6
    
    /*!  \brief Habilita o watchdog */
    #define WDT_FEED (WDTCTL = WDT_MDLY_32)
    
    /*!  \brief Pino de TX em alto */
    #define TX_HIGH (TX_POUT &= ~TX_BIT)
    
    /*!  \brief Pino de TX em baixo */
    #define TX_LOW (TX_POUT |= TX_BIT)
    
    /*!  \brief Delay de aproximadamente o tamanho de um pacote */
    #define DELAY 64
    
    /*!  \brief Estrutura com os dados do sensor que ser�o transmitidos */
    #pragma pack(1)
    typedef struct SENSOR_DATA_ST
    {
      unsigned char identificador[4];
      unsigned char tipo;
      unsigned char valor[2];
      unsigned char chk;
    }SENSOR_DATA;
    
    //Prot�tipo das fun��es de escopo local
    static void serialInit(void);
    static void serialInitIO(void);
    static void btInitIO(void);
    static void adc10Init(void);
    static void clockInit(void);
    static void timerInit(void);
    static unsigned char chkCalc(unsigned char *,unsigned char);
    
    /*!  \brief Armazena os dados que ser�o enviados */
    SENSOR_DATA data;
    
    /*!  \brief Armazena o valor atual do sensor */
    unsigned char sensorVal = 1;
    
    /*!  \brief Debounce state machine */
    unsigned char dbSt = 0;
    
    /*!  \brief Contador para rotina de debounce */
    unsigned char dbCount = 0;
    
    /*!  \brief Indica se � necess�rio transmitir um bytes com zero */
    unsigned char dbTxOffPending = 0;
    
    /*!  \brief Ponteiro para os dados que ser�o enviados */
    unsigned char * dataPt = (unsigned char *)(&data);
    
    /*!  \brief N�mero de bytes j� transmitidos no pacote */
    unsigned char countSendBytes = 0;
    
    /*!  \brief N�mero de bits j� transmitidos em um determinado byte */
    unsigned char countSendBits = 0;
    
    /*!  \brief Armazena estado da m�quina de comunica��o serial */
    unsigned char txState = 0;
    
    /*!  \brief Contador dos tempo de delay */
    unsigned char countDelay = 0;
    
    /*!  \brief Variavel temporaria para o calculo da temperatura */
    long temp;
    
    /*!  \brief Valor da temperatura em oC */
    volatile long IntDegC;
    
    /*!  \brief valor calibrado do slope do sensor de temperatura */
    long tempSlope;
    
    /*!  \brief valor calibrado do 0degC calibrado */
    long temp0degC;
    
    /*!  \brief Sinaliza que tem novo valor de temperatura */
    volatile unsigned char tempReady = 0;
    
    #pragma segment="ID_ADDR"
    const volatile unsigned char * NUMERO_SERIE = (unsigned char const volatile *)0xF800; //{0x00,0x00,0x00,0x07};
    
    void main(void)
    {
       //Para watchdog
       WDTCTL = WDTPW + WDTHOLD;
    
       //Inicia DCO
       clockInit();
    
       //Inicia perif�ricos
       adc10Init();
       btInitIO();
       serialInit();
       
       // calcula os parametros do sensor de temperatura
       tempSlope = ((CAL_ADC_15T85 - CAL_ADC_15T30) * 1000L)/55; // slope * 1000
       temp0degC = CAL_ADC_15T30 - ((tempSlope * 30)/1000);     // valor de referencia para 0degC
       
       //Inicia o watchdog
       WDT_FEED;
    
       //Modo de baixo consumo com interrup��o habilitada
       __enable_interrupt();
       ADC10CTL0 |= ENC + ADC10SC;             // Sampling and conversion start
    
       while(1)
       {
          
          __bis_SR_register(CPUOFF + GIE);        // LPM0 with interrupts enabled
          
          if (tempReady)
          {
             tempReady = 0;
             
             // calibracao da leitura do ADC
             // ADC (corrected) =( (ADC(raw) x CAL_ADC15VREF_FACTOR / 2^15) x CAL_ADC_GAIN_FACTOR / 2^15 )+ CAL_ADC_OFFSET
             temp = ADC10MEM;
             temp = (temp * CAL_ADC_15VREF_FACTOR) / 32767; // ajuste do VREF
             temp = (temp * CAL_ADC_GAIN_FACTOR) / 32767;       // ajuste do fator de ganho
             temp += CAL_ADC_OFFSET;                            // ajuste do offset
             
             // calculo da temperatura
             IntDegC = (((temp - temp0degC) * 10000) / tempSlope);
             // oC = ((A10/1024)*1500mV)-986mV)*1/3.55mV = A10*423/1024 - 278
             //IntDegC = ((temp - 673) * 423) / 1024;
    
             __no_operation();                       // SET BREAKPOINT HERE
          
             ADC10CTL0 |= ENC + ADC10SC;             // Sampling and conversion start
          }
      }
    }
    
    /*!  \brief Configura o DCO do MSP */
    static void clockInit(void)
    {
      //DCO em 1 MHz
      BCSCTL1= CALBC1_1MHZ;
      DCOCTL = CALDCO_1MHZ;
    }
    
    /*!  \brief Configura o hw do timer */
    static void timerInit(void)
    {
      //Habilita interrup��o
      TACCTL0 = CCIE;
    
      //Define o per�odo com sendo o tempo de bit dos dados
      TACCR0 = TIMER_CNTR;
      TACTL = TASSEL_2 + MC_1;
    }
    
    /*!  \brief Configura o hw da serial e o timer */
    static void serialInit(void)
    {
       serialInitIO();
       timerInit();
    
       //Preenche a estrutura
       data.identificador[0] = NUMERO_SERIE[0];
       data.identificador[1] = NUMERO_SERIE[1];
       data.identificador[2] = NUMERO_SERIE[2];
       data.identificador[3] = NUMERO_SERIE[3];
    
       data.tipo = TIPO_ANALOGICO;
    }
    
    /*!  \brief Configura os pinos de transmiss�o do sensor */
    static void serialInitIO(void)
    {
      //Configura pino como IO
      TX_PSEL &= ~TX_BIT;
      TX_PSEL &= ~TX_PULL;
    
      //Configura pino como sa�da em n�vel alto
      TX_PDIR |= TX_BIT;
      TX_HIGH;
    
      //Configura Pull up como sa�da em n�vel alto
      TX_PDIR |= TX_PULL;
      TX_POUT |= TX_PULL;
    }
    
    /*!  \brief Configura o pino conectado ao bot�o */
    static void btInitIO(void)
    {
      //Configura como GPIO e entrada
      BT_PSEL &= ~BT_BIT;
      BT_PDIR &= ~BT_BIT;
    }
    
    /*! \brief Inicializa o ADC10 para medir a temperatura */
    static void adc10Init(void)
    {
       ADC10CTL1 = INCH_10 + ADC10DIV_3;         // Temp Sensor ADC10CLK/4
       ADC10CTL0 = SREF_1 + ADC10SHT_3 + REFON + ADC10ON + ADC10IE;
    }
    
    // ADC10 interrupt service routine
    #pragma vector=ADC10_VECTOR
    __interrupt void ADC10_ISR(void)
    {
      __bic_SR_register_on_exit(CPUOFF);        // Clear CPUOFF bit from 0(SR)
      tempReady = 1;
    }
    
    // Timer A0 interrupt service routine
    #pragma vector=TIMER0_A0_VECTOR
    __interrupt void Timer_A (void)
    {
      WDT_FEED;
    
      switch(dbSt)
      {
        case 0:
          if(BT_PIN & BT_BIT)
          {
            dbCount++;
            if(dbCount >= DB_LIMIT)
            {
              dbTxOffPending = 1;
              sensorVal = 0;
              dbSt = 1;
            }
          }
          else
          {
            dbCount = 0;
            sensorVal = 1;
          }
        break;
    
        case 1:
          if(!(BT_PIN & BT_BIT))
          {
            dbCount++;
            if(dbCount >= DB_LIMIT)
            {
              dbSt = 0;
              sensorVal = 1;
            }
          }
          else
          {
            dbCount = 0;
            sensorVal = 0;
          }
        break;
      }
    
      switch(txState)
      {
        case START_BIT:
          TX_LOW;
          countSendBits = 0;
          countSendBytes = 0;
          txState = SEND_DATA;
    
          data.valor[0] = (IntDegC>>8) & 0x00FF;
          data.valor[1] = (IntDegC) & 0x00FF;
    
    
          //Calcula o checksum dos dados
          data.chk = (unsigned char)chkCalc((unsigned char *)(&data),7);
        break;
    
        case SEND_DATA:
          if(dataPt[countSendBytes] & (1 << (7 - countSendBits)))
          {
            TX_HIGH;
          }
          else
          {
            TX_LOW;
          }
    
          countSendBits++;
    
          if(countSendBits > 7)
          {
            countSendBits = 0;
            countSendBytes++;
            txState = RESYNC_HIGH;
          }
    
          if(countSendBytes > 7)
          {
            countSendBytes++;
            txState = STOP_BIT;
          }
        break;
    
        case RESYNC_HIGH:
            TX_HIGH;
            txState = RESYNC_LOW;
        break;
    
        case RESYNC_LOW:
            TX_LOW;
            txState = SEND_DATA;
        break;
    
        case STOP_BIT:
          TX_HIGH;
          txState = TX_WAIT;
          countDelay = 0;
        break;
    
        case TX_WAIT:
          if(++countDelay > DELAY)
          {
            txState = START_BIT;
          }
        break;
    
        default:
          txState = START_BIT;
        break;
      }
      __bic_SR_register_on_exit(CPUOFF);        // Clear CPUOFF bit from 0(SR)
    }
    
    /*!  \brief Calcula o checksum dos dados do identificador
     *   \param pmsg Ponteiro para os dados do identificador
     *   \param msgSize Quantidade de bytes do identificador
     */
    static unsigned char chkCalc(unsigned char * pmsg,unsigned char msgSize)
    {
      unsigned int chk;
      unsigned char i;
    
      chk = 0;
      for(i=0;i<msgSize;i++)
      {
        chk += pmsg[i];
      }
    
      return (unsigned char)chk;
    }

  • Thank you!

    That really helped!

    Sincerely,

    Larissa.

**Attention** This is a public forum