Hello
first- a quick thanks for all advice up until now. Project is going along nicely, all roadblocks you folks have helped me get passed.  Much thanks!
Two processor system. Initially it was an 8051 Master with a MSP3000 family ( i think maybe 2000 family)
I am replacing hte 8051 with a MSP430f5659
i have a compile file - I dont know what to call it - who defines what compiles to run based on a macro type definition.
I need an
#if (defined __ ??__)
statement for the compiler I'm using - the IAR version 6.1 compiler, but I dont know how to specifically do that. I have tried to look this up in the compiler users guide - no luck. tried google, a number of places, no luck.
My boss wants this code to be compile-able with an old processor or new, so he wants this file to add the new option, which I'm making MASTER2. So MASTER2 will the preprocessor directives for the MSP430f5659 so I will add an
#elif (defined __???__)
#define MASTER2
Anyone have any idea what the ??? will be, and can I discriminate between the old msp, I believe it's a 3000 family or so, and my msp 5000 family so it won't try to compile the wrong processor with the wrong compiler? The slave processor uses an IAR compiler as well, but an older version.
thanks!
Dubs
The file currently being used read as listed below:
/*------------------*/
/*--- IAR MSP430 ---*/
/*------------------*/
#if (defined __ICC430__)
 #define SLAVE
#include <msp430x44x.h>
#define codeconst(T) const T
...
#elif (defined __C51__)
 #define MASTER
#undef FALSE // in Keil 8.09, the uPSD header file defines these!
 #undef OFF // bad Keil for changing something like that
 #undef TRUE
...
/*------------------*/
/*--- BORLAND C ---*/
/*------------------*/
#elif (defined __BORLANDC__)
#define xdata
 #define idata
...
#else
 #error "unknown compiler/target"
#endif
MSP430f5659