I have been using the CC3100 SDK to develop a project and have had it running successfully for a while. I recently decided to power the MSP430F5529LP LaunchPad from a USB charger and that is when things started getting weird. I have tried running the same code as before but now the I2C clock looks like a disorganized mess.
If, however, I comment out the functions that set up the CC3100 (SPI) and CLI_WRITE (UART) and only run the I2C code I have no issue (the clock setting does not affect anything) . The same applies if I disable the I2C code and run the other half of the code. The confusing part is the code DID WORK for the better part of a day with almost no issues (only issue was AP connection dropped after ~5 minutes). If anyone has any possible insight as to what may have happened to cause this I would be happy to hear ANY suggestions. I have tried Reinstalling CCS, the SDK and even reflashed the CC3100BOOST.
I did post this originally in the SimpleLink forum but after a long while they have suggested I try see if you guys have any explanation a why now I2C is not working at all.
Thankfully
Kas
My Code:
/*
* main.c - TCP socket sample application
*
* Copyright (C) 2014 Texas Instruments Incorporated - http://www.ti.com/
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/*
* Application Name - TCP socket
* Application Overview - This is a sample application demonstrating how to open
* and use a standard TCP socket with CC3100.
* Application Details - http://processors.wiki.ti.com/index.php/CC31xx_TCP_Socket_Application
* doc\examples\tcp_socket.pdf
*/
#include "simplelink.h"
#include "cli_uart.h"
#include <msp430.h>
#define APPLICATION_VERSION "1.0.0"
/**/
#define LOOP_FOREVER(line_number) \
{\
while(1); \
}
#define ASSERT_ON_ERROR(line_number, error_code) \
{\
/* Handling the error-codes is specific to the application */ \
if (error_code < 0) return error_code; \
/* else, continue w/ execution */ \
}
/*
* Values for below macros shall be modified per the access-point's (AP) properties
* SimpleLink device will connect to following AP when the application is executed
*/
// #define SSID_NAME "" /* AP name to connect to. */
// #define SEC_TYPE SL_SEC_TYPE_WPA /* Security type of the Access piont */
// #define PASSKEY "" /* Password in case of secure AP */
// #define IP_ADDR //TODO: Change to a passed in value
// #define PORT_NUM 5001 /* Port number to be used */
#define SSID_NAME "" /* AP name to connect to. */
#define SEC_TYPE SL_SEC_TYPE_WPA /* Security type of the Access piont */
#define PASSKEY "" /* Password in case of secure AP */
#define IP_ADDR //TODO: Change to a passed in value
#define PORT_NUM 5001 /* Port number to be used */
// #define SSID_NAME "" /* AP name to connect to. */
// #define SEC_TYPE SL_SEC_TYPE_WPA /* Security type of the Access point */
// #define PASSKEY "" /* Password in case of secure AP */
//#define IP_ADDR //TODO: Change to a passed in value
//#define PORT_NUM 5001 /* Port number to be used */
#define IP_ADDR 0x6b15d6c7//Plotly
#define PORT_NUM 80//Plotly /* Port number to be used */
#define BUF_SIZE 1400
#define NO_OF_PACKETS 10
#define SUCCESS 0
/* Status bits - These are used to set/reset the corresponding bits in a 'status_variable' */
typedef enum{
STATUS_BIT_CONNECTION = 0, /* If this bit is:
* 1 in a 'status_variable', the device is connected to the AP
* 0 in a 'status_variable', the device is not connected to the AP
*/
STATUS_BIT_IP_AQUIRED /* If this bit is:
* 1 in a 'status_variable', the device has acquired an IP
* 0 in a 'status_variable', the device has not acquired an IP
*/
}e_StatusBits;
/* Application specific status/error codes */
typedef enum{
DEVICE_NOT_IN_STATION_MODE = -0x7D0, /* Choosing this number to avoid overlap w/ host-driver's error codes */
STATUS_CODE_MAX = -0xBB8
}e_AppStatusCodes;
#define SET_STATUS_BIT(status_variable, bit) status_variable |= (1<<(bit))
#define CLR_STATUS_BIT(status_variable, bit) status_variable &= ~(1<<(bit))
#define GET_STATUS_BIT(status_variable, bit) (0 != (status_variable & (1<<(bit))))
#define IS_CONNECTED(status_variable) GET_STATUS_BIT(status_variable, \
STATUS_BIT_CONNECTION)
#define IS_IP_AQUIRED(status_variable) GET_STATUS_BIT(status_variable, \
STATUS_BIT_IP_AQUIRED)
/*
* GLOBAL VARIABLES -- Start
*/
union
{
UINT8 BsdBuf[BUF_SIZE];
UINT32 demobuf[BUF_SIZE/4];
} uBuf;
UINT8 g_Status = 0;
/****************************************CARRIED OVER START*/
unsigned char *PTxData; // Pointer to TX data
unsigned char TXByteCtr;
unsigned char *PRxData; // Pointer to RX data
unsigned char RXByteCtr;
unsigned char RxBuffer[128]; // Allocate 128 byte of RAM
char multiple;
char stopBit = FALSE;
/****************************************CARRIED OVER END*/
char xValue[] = "\0\0\0\0\0\0";
unsigned char errorArray[] = "\0\0\0\0\0\0\0\0\0\0";
int connectedToAP = 0;
int connetcedToSocket = 0;
/*
* GLOBAL VARIABLES -- End
*/
/*
* STATIC FUNCTION DEFINITIONS -- Start
*/
void clearErrorArray();
static INT32 configureSimpleLinkToDefaultState();
static INT32 establishConnectionWithAP();
void configureCC3x00();
void startCC3x00();
void connectCC3x00();
//static INT16 BsdTcpServer(UINT16 Port);
static INT16 BsdTcpClient(UINT16 Port);
static INT16 packetTx(UINT16 socketID, unsigned char* message, int length, char closeSocket);
static INT32 initializeAppVariables();
static void displayBanner();
int intToChars(int number, char* chars);
int charToInt(signed char value);
void hexByteToChar(char byteIn, char* nibbleA, char* nibbleB);
int plotlyPlotString(int xVal, int yVal, char* dataStream);
void I2CInit();
void I2CTx(unsigned char* TxData, unsigned char numBytes, char stop);
void I2CRx(unsigned char* RxBuffer, unsigned char numBytes);
int mpl3115aInit();
int mpl3115aRead();
/*
* STATIC FUNCTION DEFINITIONS -- End
*/
/*
* ASYNCHRONOUS EVENT HANDLERS -- Start
*/
/*!
\brief This function handles WLAN events
\param[in] pWlanEvent is the event passed to the handler
\return None
\note
\warning
*/
void SimpleLinkWlanEventHandler(SlWlanEvent_t *pWlanEvent)//TODO: Look at all the possible events that can occur and decide if other events need to be handled
{
switch(pWlanEvent->Event)
{
case SL_WLAN_CONNECT_EVENT:
{
SET_STATUS_BIT(g_Status, STATUS_BIT_CONNECTION);
intToChars(pWlanEvent->Event, errorArray);
CLI_Write(" STATUS_BIT_CONNECTION Value: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
/*
* Information about the connected AP (like name, MAC etc) will be
* available in 'sl_protocol_wlanConnectAsyncResponse_t' - Applications
* can use it if required
*
* sl_protocol_wlanConnectAsyncResponse_t *pEventData = NULL;
* pEventData = &pWlanEvent->EventData.STAandP2PModeWlanConnected;
*
*/
}
break;
case SL_WLAN_DISCONNECT_EVENT:
{
sl_protocol_wlanConnectAsyncResponse_t* pEventData = NULL;
CLR_STATUS_BIT(g_Status, STATUS_BIT_CONNECTION);
CLR_STATUS_BIT(g_Status, STATUS_BIT_IP_AQUIRED);
pEventData = &pWlanEvent->EventData.STAandP2PModeDisconnected;
/* If the user has initiated 'Disconnect' request, 'reason_code' is
* SL_USER_INITIATED_DISCONNECTION */
if(SL_USER_INITIATED_DISCONNECTION == pEventData->reason_code)//TODO: Add connection flag here to be checked in main loop and reconnect should a connection error occur
{
CLI_Write(" Device disconnected from the AP on application's request \n\r");
intToChars(pWlanEvent->Event, errorArray);
CLI_Write(" Error Code A.0: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
connectedToAP = 0;
intToChars(pEventData->reason_code, errorArray);
CLI_Write(" Error Code A.1: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
}
else
{
CLI_Write(" Device disconnected from the AP on an ERROR..!! \n\r");
connectedToAP = 0;
intToChars(pWlanEvent->Event, errorArray);
CLI_Write(" Error Code A.2: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
connectedToAP = 0;
intToChars(pEventData->reason_code, errorArray);
CLI_Write(" Error Code A.3: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
}
}
break;
default:
{
CLI_Write(" [WLAN EVENT] Unexpected event \n\r");
connectedToAP = 0;
intToChars(pWlanEvent->Event, errorArray);
CLI_Write(" Error Code B: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
}
break;
}
}
/*!
\brief This function handles events for IP address acquisition via DHCP
indication
\param[in] pNetAppEvent is the event passed to the handler
\return None
\note
\warning
*/
void SimpleLinkNetAppEventHandler(SlNetAppEvent_t *pNetAppEvent)
{
switch(pNetAppEvent->Event)
{
case SL_NETAPP_IPV4_ACQUIRED:
{
SET_STATUS_BIT(g_Status, STATUS_BIT_IP_AQUIRED);
intToChars(pNetAppEvent->Event, errorArray);
CLI_Write(" Event Value: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
intToChars(STATUS_BIT_IP_AQUIRED, errorArray);
CLI_Write(" STATUS_BIT_IP_AQUIRED Value: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
/*
* Information about the connection (like IP, gateway address etc)
* will be available in 'SlIpV4AcquiredAsync_t'
* Applications can use it if required
*
* SlIpV4AcquiredAsync_t *pEventData = NULL;
* pEventData = &pNetAppEvent->EventData.ipAcquiredV4;
*
*/
}
break;
default:
{
CLI_Write(" [NETAPP EVENT] Unexpected event \n\r");
intToChars(pNetAppEvent->Event, errorArray);
CLI_Write(" Error Code C: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
}
break;
}
}
/*!
\brief This function handles callback for the HTTP server events
\param[in] pServerEvent - Contains the relevant event information
\param[in] pServerResponse - Should be filled by the user with the
relevant response information
\return None
\note
\warning
*/
void SimpleLinkHttpServerCallback(SlHttpServerEvent_t *pHttpEvent,
SlHttpServerResponse_t *pHttpResponse)
{
/* Unused in this application */
CLI_Write(" [HTTP EVENT] Unexpected event \n\r");
}
/*!
\brief This function handles general error events indication
\param[in] pDevEvent is the event passed to the handler
\return None
*/
void SimpleLinkGeneralEventHandler(SlDeviceEvent_t *pDevEvent)
{
/*
* Most of the general errors are not FATAL are are to be handled
* appropriately by the application
*/
CLI_Write(" [GENERAL EVENT] \n\r");
intToChars(pDevEvent->Event, errorArray);
CLI_Write(" Error Code D: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
}
/*!
\brief This function handles socket events indication
\param[in] pSock is the event passed to the handler
\return None
*/
void SimpleLinkSockEventHandler(SlSockEvent_t *pSock)
{
switch( pSock->Event )
{
case SL_NETAPP_IPV4_ACQUIRED:
//TODO: Fill in needed code here (set flag)
break;
case SL_NETAPP_SOCKET_TX_FAILED:
/*
* TX Failed
*
* Information about the socket descriptor and status will be
* available in 'SlSockEventData_t' - Applications can use it if
* required
*
* SlSockEventData_t *pEventData = NULL;
* pEventData = & pSock->EventData;
*/
switch( pSock->EventData.status )
{
case SL_ECLOSE:
CLI_Write(" [SOCK EVENT] Close socket operation failed to transmit all queued packets\n\r");
connetcedToSocket = 0;
intToChars(pSock->Event, errorArray);
CLI_Write(" Error Code E: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
break;
default:
CLI_Write(" [SOCK EVENT] Unexpected event 1\n\r");
connetcedToSocket = 0;
intToChars(pSock->Event, errorArray);
CLI_Write(" Error Code F: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
break;
}
break;
default:
CLI_Write(" [SOCK EVENT] Unexpected event 2\n\r");
connetcedToSocket = 0;
intToChars(pSock->Event, errorArray);
CLI_Write(" Error Code G: ");
CLI_Write(errorArray);
CLI_Write("\r\n\r\n");
clearErrorArray();
break;
}
}
/*
* ASYNCHRONOUS EVENT HANDLERS -- End
*/
void clearErrorArray(){
char i;
for(i = 0; i < 12; i++){
errorArray[i] = '\0';
}
}
/*!
\brief This function configure the SimpleLink device in its default state. It:
- Sets the mode to STATION
- Configures connection policy to Auto and AutoSmartConfig
- Deletes all the stored profiles
- Enables DHCP
- Disables Scan policy
- Sets Tx power to maximum
- Sets power policy to normal
- Unregisters mDNS services
\param[in] none
\return On success, zero is returned. On error, negative is returned
*/
static INT32 configureSimpleLinkToDefaultState()
{
SlVersionFull ver = {0};
UINT8 val = 1;
UINT8 configOpt = 0;
UINT8 configLen = 0;
UINT8 power = 0;
INT32 retVal = -1;
INT32 mode = -1;
mode = sl_Start(0, 0, 0);
ASSERT_ON_ERROR(__LINE__, mode);
/* If the device is not in station-mode, try configuring it in staion-mode */
if (ROLE_STA != mode)
{
if (ROLE_AP == mode)
{
/* If the device is in AP mode, we need to wait for this event before doing anything */
while(!IS_IP_AQUIRED(g_Status)) { _SlNonOsMainLoopTask(); }
}
/* Switch to STA role and restart */
retVal = sl_WlanSetMode(ROLE_STA);
ASSERT_ON_ERROR(__LINE__, retVal);
retVal = sl_Stop(0xFF);
ASSERT_ON_ERROR(__LINE__, retVal);
retVal = sl_Start(0, 0, 0);
ASSERT_ON_ERROR(__LINE__, retVal);
/* Check if the device is in station again */
if (ROLE_STA != retVal)
{
/* We don't want to proceed if the device is not coming up in station-mode */
return DEVICE_NOT_IN_STATION_MODE;
}
}
/* Get the device's version-information */
configOpt = SL_DEVICE_GENERAL_VERSION;
configLen = sizeof(ver);
retVal = sl_DevGet(SL_DEVICE_GENERAL_CONFIGURATION, &configOpt, &configLen, (unsigned char *)(&ver));
ASSERT_ON_ERROR(__LINE__, retVal);
/* Set connection policy to Auto + SmartConfig (Device's default connection policy) */
retVal = sl_WlanPolicySet(SL_POLICY_CONNECTION, SL_CONNECTION_POLICY(1, 0, 0, 0, 1), NULL, 0);
ASSERT_ON_ERROR(__LINE__, retVal);
/* Remove all profiles */
retVal = sl_WlanProfileDel(0xFF);
ASSERT_ON_ERROR(__LINE__, retVal);
/*
* Device in station-mode. Disconnect previous connection if any
* The function returns 0 if 'Disconnected done', negative number if already disconnected
* Wait for 'disconnection' event if 0 is returned, Ignore other return-codes
*/
retVal = sl_WlanDisconnect();
if(0 == retVal)
{
/* Wait */
while(IS_CONNECTED(g_Status)) { _SlNonOsMainLoopTask(); }
}
/* Enable DHCP client*/
retVal = sl_NetCfgSet(SL_IPV4_STA_P2P_CL_DHCP_ENABLE,1,1,&val);
ASSERT_ON_ERROR(__LINE__, retVal);
/* Disable scan */
configOpt = SL_SCAN_POLICY(0);
retVal = sl_WlanPolicySet(SL_POLICY_SCAN , configOpt, NULL, 0);
ASSERT_ON_ERROR(__LINE__, retVal);
/* Set Tx power level for station mode
Number between 0-15, as dB offset from max power - 0 will set maximum power */
power = 0;
retVal = sl_WlanSet(SL_WLAN_CFG_GENERAL_PARAM_ID, WLAN_GENERAL_PARAM_OPT_STA_TX_POWER, 1, (unsigned char *)&power);
ASSERT_ON_ERROR(__LINE__, retVal);
/* Set PM policy to normal */
retVal = sl_WlanPolicySet(SL_POLICY_PM , SL_NORMAL_POLICY, NULL, 0);
ASSERT_ON_ERROR(__LINE__, retVal);
/* Unregister mDNS services */
retVal = sl_NetAppMDNSUnRegisterService(0, 0);
ASSERT_ON_ERROR(__LINE__, retVal);
retVal = sl_Stop(0xFF);
ASSERT_ON_ERROR(__LINE__, retVal);
retVal = initializeAppVariables();
ASSERT_ON_ERROR(__LINE__, retVal);
return retVal; /* Success */
}
/*!
\brief Connecting to a WLAN Access point
This function connects to the required AP (SSID_NAME).
The function will return once we are connected and have acquired IP address
\param[in] None
\return 0 on success, negative error-code on error
\note
\warning If the WLAN connection fails or we don't acquire an IP address,
We will be stuck in this function forever.
*/
static INT32 establishConnectionWithAP()
{
SlSecParams_t secParams = {0};
INT32 retVal = 0;
secParams.Key = PASSKEY;
secParams.KeyLen = strlen(PASSKEY);
secParams.Type = SEC_TYPE;
retVal = sl_WlanConnect(SSID_NAME, strlen(SSID_NAME), 0, &secParams, 0);
ASSERT_ON_ERROR(__LINE__, retVal);
/* Wait */
while((!IS_CONNECTED(g_Status)) || (!IS_IP_AQUIRED(g_Status))) { _SlNonOsMainLoopTask(); }
connectedToAP = 1;//TODO: remove flag
return SUCCESS;
}
/****************************************************************************************************************************************/
/*
* Following function configures the device to default state by cleaning
* the persistent settings stored in NVMEM (viz. connection profiles &
* policies, power policy etc)
*
* Applications may choose to skip this step if the developer is sure
* that the device is in its default state at start of application
*
* Note that all profiles and persistent settings that were done on the
* device will be lost
*/
void configureCC3x00(){
INT32 retVal = -1;
retVal = configureSimpleLinkToDefaultState();
if(retVal < 0)
{
if (DEVICE_NOT_IN_STATION_MODE == retVal)
{
CLI_Write(" Failed to configure the device in its default state \n\r");
}
LOOP_FOREVER(__LINE__);
}
CLI_Write(" Device is configured in default state \n\r");
}
/*
* Assumption is that the device is configured in station mode already
* and it is in its default state
*/
/* Initializing the CC3100 device */
void startCC3x00(){
INT32 retVal = -1;
retVal = sl_Start(0, 0, 0);
if ((retVal < 0) ||
(ROLE_STA != retVal) )
{
CLI_Write(" Failed to start the device \n\r");
LOOP_FOREVER(__LINE__);
}
CLI_Write(" Device started as STATION \n\r");
}
/* Connecting to WLAN AP - Set with static parameters defined at the top
After this call we will be connected and have IP address */
void connectCC3x00(){
INT32 retVal = -1;
retVal = establishConnectionWithAP();
if(retVal < 0)
{
CLI_Write(" Failed to establish connection w/ an AP \n\r");
LOOP_FOREVER(__LINE__);
}
CLI_Write(" Connection established w/ AP and IP is acquired \n\r");
}
/*!
\brief Opening a client side socket and sending data
This function opens a TCP socket and tries to connect to a Server IP_ADDR
waiting on port PORT_NUM. If the socket connection is successful then the
function will send 1000 TCP packets to the server.
\param[in] port number on which the server will be listening on
\return 0 on success, -1 on Error.
\note
\warning A server must be waiting with an open TCP socket on the
right port number before calling this function.
Otherwise the socket creation will fail.
*/
static INT16 BsdTcpClient(UINT16 Port)
{
SlSockAddrIn_t Addr;
UINT16 AddrSize = 0;
INT16 SockID = 0;
INT16 Status = 0;
Addr.sin_family = SL_AF_INET;
Addr.sin_port = sl_Htons((UINT16)Port);
Addr.sin_addr.s_addr = sl_Htonl((UINT32)IP_ADDR);//TODO: Change this as a passed in value(Keep as defined for current version)
AddrSize = sizeof(SlSockAddrIn_t);
SockID = sl_Socket(SL_AF_INET,SL_SOCK_STREAM, 0);
if( SockID < 0 )
{
/* error */
return -1;
}
CLI_Write(" Establishing connection with TCP server \n\r");
Status = sl_Connect(SockID, ( SlSockAddr_t *)&Addr, AddrSize);
if( Status < 0 )
{
sl_Close(SockID);
CLI_Write(" Failed to establish connection with TCP server \n\r");
return -1;
}
CLI_Write(" Connection with TCP server established successfully \n\r");
connetcedToSocket = 1;//TODO: remove flag
return SockID;
}
static INT16 packetTx(UINT16 socketID, unsigned char* message, int length, char closeSocket){
INT16 Status = 0;
INT8 sent = -1;
INT8 i = 0;
INT16 j = 0;
CLI_Write(" - Initiating message transmit\n\r");
while((sent == -1) && (i < 6)){
Status = sl_Send(socketID, message, length, 0 );
sent = Status;
i++;
if (sent != 0){
for (j = 0; j < 1000; j++);
}
}
if( Status < 0 )
{
CLI_Write(" Error while sending the data \n\r");
sl_Close(socketID);
return -1;
}
CLI_Write(" - Message transmitted\n\r");
//// if (closeSocket == 1){
// sl_Close(socketID);//TODO: Remove close socket
//// }
return 0;
}
/*!
\brief This function initializes the application variables
\param[in] None
\return 0 on success, negative error-code on error
*/
static INT32 initializeAppVariables()
{
g_Status = 0;
memset(uBuf.BsdBuf, 0, sizeof(uBuf));
return SUCCESS;
}
/*!
\brief This function displays the application's banner
\param None
\return None
*/
static void displayBanner()
{
CLI_Write("\n\r\n\r");
CLI_Write(" TCP socket application - Version ");
CLI_Write(APPLICATION_VERSION);
CLI_Write("\n\r*******************************************************************************\n\r");
}
int intToChars(int number, char* chars){
int val = number;
int i = 0;
int j = 0;
int num;
int neg = 0;
char temp;
if (val < 0){
val = 0 - val;
neg = 1;
}
if (val == 0){
chars[0] = '0';
i = 1;
}
while(val != 0){
num = val/10;
chars[i] = (char)(val - (num * 10) + 0x30);
val = num;
i++;
}
i--;//Remove extra count
int f;
if (i % 2 != 0){
f = i / 2 + 1;
}
else {
f = i / 2;
}
for (j = 0; j < f; j++){
temp = chars[j];
chars[j] = chars[i - j];
chars[i - j] = temp;
}
if (neg){
for (j = i; j >= 0; j--){
chars[j + 1] = chars[j];
}
chars[0] = '-';
i++;//increase count to account for negitive sign
}
return i + 1; //Counting from zero so add one for true length
}
//Converts Hex representation to characters
int charToInt(signed char value){
int mambo = 0;
if (value < 0){
value = 0 - value;
mambo = 0 - (int)value;
}
else{
mambo = (int)value;
}
return mambo;
}
void hexByteToChar(char byteIn, char* nibbleA, char* nibbleB)
{
switch(byteIn & 0xF0){
case 0x0:
*nibbleA = '0';
break;
case 0x10:
*nibbleA = '1';
break;
case 0x20:
*nibbleA = '2';
break;
case 0x30:
*nibbleA = '3';
break;
case 0x40:
*nibbleA = '4';
break;
case 0x50:
*nibbleA = '5';
break;
case 0x60:
*nibbleA = '6';
break;
case 0x70:
*nibbleA = '7';
break;
case 0x80:
*nibbleA = '8';
break;
case 0x90:
*nibbleA = '9';
break;
case 0xA0:
*nibbleA = 'A';
break;
case 0xB0:
*nibbleA = 'B';
break;
case 0xC0:
*nibbleA = 'C';
break;
case 0xD0:
*nibbleA = 'D';
break;
case 0xE0:
*nibbleA = 'E';
break;
case 0xF0:
*nibbleA = 'F';
break;
}
switch (byteIn & 0x0F){
case 0x00:
*nibbleB = '0';
break;
case 0x01:
*nibbleB = '1';
break;
case 0x02:
*nibbleB = '2';
break;
case 0x03:
*nibbleB = '3';
break;
case 0x04:
*nibbleB = '4';
break;
case 0x05:
*nibbleB = '5';
break;
case 0x06:
*nibbleB = '6';
break;
case 0x07:
*nibbleB = '7';
break;
case 0x08:
*nibbleB = '8';
break;
case 0x09:
*nibbleB = '9';
break;
case 0x0A:
*nibbleB = 'A';
break;
case 0x0B:
*nibbleB = 'B';
break;
case 0x0C:
*nibbleB = 'C';
break;
case 0x0D:
*nibbleB = 'D';
break;
case 0x0E:
*nibbleB = 'E';
break;
case 0x0F:
*nibbleB = 'F';
break;
}
}
int plotlyPlotString(int xVal, int yVal, char* dataStream){
const char start[] = "\r\n{\"x\":";
const char middle[] = ",\"y\":";
const char end[] = "}\r\n";
// char xValue[] = "\0\0\0\0\0\0";
char yValue[] = "\0\0\0\0\0\0";
intToChars(xVal, xValue);
intToChars(yVal, yValue);
int offset = 4;
strncpy(dataStream + offset, start, sizeof(start) - 1);
offset = offset + sizeof(start) - 1;
strncpy(dataStream + offset, xValue, strlen(xValue));
offset = offset + strlen(xValue);
strncpy(dataStream + offset, middle, sizeof(middle) - 1);
offset = offset + sizeof(middle) - 1;
strncpy(dataStream + offset, yValue, strlen(yValue));
offset = offset + strlen(yValue);
strncpy(dataStream + offset, end, sizeof(end)); //Leave out the -1 inorder to include the null terminator
int streamLength;
char streamDataLen[] = "\0\0\0\0\0";
streamLength = sizeof(start) - 2 + strlen(xValue) + sizeof(middle) + strlen(yValue) + sizeof(end) - 3;
intToChars(streamLength, streamDataLen);
char happyDay[4];
hexByteToChar(streamDataLen[0], happyDay, happyDay + 1);
hexByteToChar(streamDataLen[1], happyDay + 2, happyDay + 3);
strncpy(dataStream, happyDay, 4);
return streamLength;
}
void I2CInit(){
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P4SEL |= 0x06; // Assign I2C pins to USCI_B0
UCB1CTL1 |= UCSWRST; // Enable SW reset
UCB1CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode
UCB1CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB1BR0 = 10; // fSCL = SMCLK/12 = ~100kHz
UCB1BR1 = 0;
UCB1I2CSA = 0x60; // Slave Address is 048h
UCB1CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
UCB1IE |= UCTXIE; // Enable TX interrupt
UCB1IE |= UCRXIE; // Enable RX interrupt
}
void I2CTx(unsigned char* TxData, unsigned char numBytes, char stop){
unsigned int i;
stopBit = stop;
for(i=0;i<10;i++); // Delay required between transaction
PTxData = (unsigned char *)TxData; // TX array start address
// Place breakpoint here to see each
// transmit operation.
TXByteCtr = numBytes; // Load TX byte counter
UCB1CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0, enable interrupts
__no_operation(); // Remain in LPM0 until all data
if(stop){
UCB1CTL1 |= UCTXSTP;
}
// is TX'd
while (UCB1CTL1 & UCTXSTP); // Ensure stop condition got sent
}
void I2CRx(unsigned char* RxBuffer, unsigned char numBytes){
PRxData = (unsigned char *)RxBuffer; // Start of RX buffer
RXByteCtr = numBytes; // Load RX byte counter
if (numBytes > 1){
multiple = 1;
}
else {
multiple = 0;
}
while (UCB1CTL1 & UCTXSTP); // Ensure stop condition got sent
UCB1CTL1 &= ~UCTR;
UCB1CTL1 |= UCTXSTT; // I2C start condition
if (multiple == 0){
while(UCB1CTL1 & UCTXSTT); // Start condition sent?
UCB1CTL1 |= UCTXSTP;
}
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0, enable interrupts
// Remain in LPM0 until all data is RX'd
__no_operation();
}
int mpl3115aInit(){
char initialized = 1;
unsigned char WHO_AM_I[] = {0x0C};
//R C4
unsigned char CTRL_REG1_SET1[] = {0x26, 0x38};
unsigned char CTRL_REG2_SET[] = {0x27, 0x00};
unsigned char CTRL_REG3_SET[] = {0x28, 0x11};
unsigned char CTRL_REG4_SET[] = {0x29, 0x00};
unsigned char CTRL_REG5_SET[] = {0x2A, 0x00};
unsigned char PT_DATA_CFG_SET[] = {0x13, 0x07};
unsigned char CTRL_REG1_GET[] = {0x26};
unsigned char CTRL_REG1_SET2[] = {0x26, 0x39};
unsigned char CTRL_REG2_GET[] = {0x27};
I2CTx(WHO_AM_I, sizeof(WHO_AM_I), FALSE);
I2CRx(RxBuffer, 1);
if (RxBuffer[0] == 0xC4){
P4OUT |= 0x80;
P1OUT &= 0xFE;
}
else {
P1OUT |= 0x01;
P4OUT &= 0x7F;
initialized = 0;
}
I2CTx(CTRL_REG1_SET1, sizeof(CTRL_REG1_SET1), TRUE);
I2CTx(CTRL_REG2_SET, sizeof(CTRL_REG2_SET), TRUE);
I2CTx(CTRL_REG3_SET, sizeof(CTRL_REG3_SET), TRUE);
I2CTx(CTRL_REG4_SET, sizeof(CTRL_REG4_SET), TRUE);
I2CTx(CTRL_REG5_SET, sizeof(CTRL_REG5_SET), TRUE);
I2CTx(PT_DATA_CFG_SET, sizeof(PT_DATA_CFG_SET), TRUE);
I2CTx(CTRL_REG1_GET, sizeof(CTRL_REG1_GET), FALSE);
I2CRx(RxBuffer, 1);
if (RxBuffer[0] == 0x38){
P4OUT |= 0x80;
P1OUT &= 0xFE;
}
else {
P1OUT |= 0x01;
P4OUT &= 0x7F;
initialized = 0;
}
I2CTx(CTRL_REG1_SET2, sizeof(CTRL_REG1_SET2), TRUE);
I2CTx(CTRL_REG1_GET, sizeof(CTRL_REG1_GET), FALSE);
I2CRx(RxBuffer, 1);
if (RxBuffer[0] == 0x39){
P4OUT |= 0x80;
P1OUT &= 0xFE;
}
else {
P1OUT |= 0x01;
P4OUT &= 0x7F;
initialized = 0;
}
I2CTx(CTRL_REG2_GET, sizeof(CTRL_REG2_GET), FALSE);
I2CRx(RxBuffer, 1);
if (RxBuffer[0] == 0x00){
P4OUT |= 0x80;
P1OUT &= 0xFE;
}
else {
P1OUT |= 0x01;
P4OUT &= 0x7F;
initialized = 0;
}
return initialized;
}
int mpl3115aRead(){
unsigned char OUT_P_MSB[] = {0x01};
unsigned char DR_STATUS[] = {0x06};
char readPresTemp = 0;
I2CTx(DR_STATUS, sizeof(DR_STATUS), FALSE);
I2CRx(RxBuffer, 1);
if ((RxBuffer[0] == 0x0E) || (RxBuffer[0] == 0xEE)){
P4OUT |= 0x80;
P1OUT &= 0xFE;
readPresTemp = 1;
}
else {
P1OUT |= 0x01;
P4OUT &= 0x7F;
readPresTemp = 0;
}
if (readPresTemp){
I2CTx(OUT_P_MSB, sizeof(OUT_P_MSB), FALSE);
I2CRx(RxBuffer, 5);
Delay(50);
}
return readPresTemp;
}
int main(void)
{
INT32 retVal = -1;
int temperatureInt;
int streamLength;
int packetLength;
char dataStream[30];
int xVal = 0;
P1OUT &= 0xFE;
P1DIR |= 0x01;
P4OUT &= 0x7F;
P4DIR |= 0x80;
retVal = initializeAppVariables();
ASSERT_ON_ERROR(__LINE__, retVal);
stopWDT();
initClk();
CLI_Configure();
CLI_Write(" \f\r\n");
displayBanner();
configureCC3x00();
startCC3x00();
connectCC3x00();
INT16 socketIDD;
socketIDD = BsdTcpClient(PORT_NUM);
packetTx(socketIDD, openStream, (sizeof(openStream) - 1), 0);
int dataAvilable;
CLI_Write(" Initilizing I2C");
I2CInit();
Delay(700);
CLI_Write(" Complete \r\n");
Delay(500);
CLI_Write(" Initilizing MPL3115A");
mpl3115aInit();
Delay(700);
CLI_Write(" Complete\r\n");
while (1)
{
dataAvilable = mpl3115aRead();
if (dataAvilable == 1){
temperatureInt = charToInt((signed char)RxBuffer[3]);
streamLength = plotlyPlotString(xVal, temperatureInt, dataStream);
packetLength = streamLength + 6;
packetTx(socketIDD, dataStream, packetLength, 0);
CLI_Write("\r\n");
CLI_Write(dataStream);
CLI_Write("\r\n");
xVal++;
}
Delay(20);
}
}
//-------------------------------------------------------------------------------
// The USCI_B0 data ISR is used to move received data from the I2C slave
// to the MSP430 memory. It is structured such that it can be used to receive
// any 2+ number of bytes by pre-loading RXByteCtr with the byte count.
//-------------------------------------------------------------------------------
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCI_B1_VECTOR
__interrupt void USCI_B1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B0_VECTOR))) USCI_B0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCB1IV,12))
{
case 0: break; // Vector 0: No interrupts
case 2: break; // Vector 2: ALIFG
case 4: break; // Vector 4: NACKIFG
case 6: break; // Vector 6: STTIFG
case 8: break; // Vector 8: STPIFG
case 10: // Vector 10: RXIFG
RXByteCtr--; // Decrement RX byte counter
if (RXByteCtr)
{
*PRxData++ = UCB1RXBUF; // Move RX data to address PRxData
if (RXByteCtr == 1 && multiple == 1) // Only one byte left?
UCB1CTL1 |= UCTXSTP; // Generate I2C stop condition
}
else
{
*PRxData = UCB1RXBUF; // Move final RX data to PRxData
__bic_SR_register_on_exit(LPM0_bits); // Exit active CPU
}
break;
case 12: // Vector 12: TXIFG
if (TXByteCtr) // Check TX byte counter
{
UCB1TXBUF = *PTxData++; // Load TX buffer
TXByteCtr--; // Decrement TX byte counter
}
else
{
if (stopBit){
UCB1CTL1 |= UCTXSTP; // I2C stop condition //Set a stop flag if this should be sent out or not
}
UCB1IFG &= ~UCTXIFG; // Clear USCI_B0 TX int flag
__bic_SR_register_on_exit(LPM0_bits); // Exit LPM0
}
default: break;
}
}