i've been able to successfully load my ez430_rf2500 using the SmartRF GUI, via a COM port...
now, i'd like to do the same thing from the command-line using the SmartRFProgConsole.exe program.... but looking at the help, there doesn't appear to be an option to select an MSP430 target ...
SmartRFProgConsole [Target][Actions][File][Interface Slow][Change / IEEE address][Flash lock][Bootloader ID]
The order of the parameters is irrelevant.
Target: [S][AU][AS][B]
S System-on-Chip (programmed via USB)
Type S(n), where n is the board ID number, to select a specific EB.
Otherwise, if there are multiple boards, the one to be programmed will be
selected at random.
AU EB application (programmed via USB)
Type AU(n), where n is the board ID number, to select a specific EB.
Otherwise, if there are multiple boards, the one to be programmed will be
selected at random.
AS(n) EB application (programmed via the EC2 adapter on serial port COMn).
(only SmartRF04EB)
B(n) EB bootloader (programmed via the EC2 adapter on serial port COMn).
(only SmartRF04EB)
in the GUI, there are *five* types of targets -- with the last being MSP430; but the command-line tool lists only *four* of the these....
is it possible to use SmartRFProgConsole to load my ez430_rf2500 from the command-line via a COM port??? and if so, what options to i need to supply??
thanks in advance....