Other Parts Discussed in Thread: MSP-EXP430FR5739, MSP430FR5739
Hi all! I'm getting started with a project on the MSP430FR5739, and I'm getting an unfamiliar compiler warning. Right now, I'm using the "MSP430FR57xx_uscia0_spi_10.asm" found in the TI Resource Explorer, and I'm having the warnings pop up in the following lines.
;-------------------------------------------------------------------------------
; Main loop here
;-------------------------------------------------------------------------------
Mainloop bis.w #LPM0+GIE,SR ; Enter LPM0 w/ interrupt
nop ; remain in LPM0
And below are the warnings that pop up:
[W0005] NOP required before set of GIE bit. #10247-D creating output section ".int56" without a SECTIONS specification #10202-D no suitable entry-point found; setting to 0
I try to ignore the warnings and run the code. It is able to locate the MSP-EXP430FR5739, and erase the memory. This error then pops up:
Load Program Error. File: C:\Users\<user>\workspace_v6_0_1\SPI_Assem\Debug\SPI_Assem.out: a data verification error occured, file load failed.
It also shows this error in the console.
MSP430: File Loader: Data verification failed at address 0x00000000 Please verify target memory and memory map. MSP430: GEL: File: C:\Users\<user>\workspace_v6_0_1\SPI_Assem\Debug\SPI_Assem.out: a data verification error occurred, file load failed.
I've looked around in the forums and user guide with no luck. I would like to know what this compiler warning actually means and, if possible, fix this issue. Thank you.