I had bought MSP-EXP430FR4133 to try out some codes and build small products based on it.I did go through the sample codes provided in MSP430ware.
I wanted to do a ADC on P8.1 and then display the Numeric code ( 0 to 1023 ) on to the LCD provided along with the Launchpad.
Apparently the LCD displays random values instead of the 10 Bit ADC one.Can some body help ?
Code is as below.
#include <msp430fr4133.h>
unsigned int sensor[2];
unsigned int splitchar[4]= { 0,0,0,0 };
unsigned int i;
unsigned int j;
const char digit[10] ={
0xFC, // "0"
0x60, // "1"
0xDB, // "2"
0xF3, // "3"
0x67, // "4"
0xB7, // "5"
0xBF, // "6"
0xE4, // "7"
0xFF, // "8"
0xF7 // "9"
};
ADC - CODES
// Configure ADC A8
SYSCFG2 |= ADCPCTL8 ;
// Disable the GPIO power-on default high-impedance mode to activate previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Configure ADC10
ADCCTL0 |= ADCSHT_1 | ADCMSC | ADCON ; // ADCON, S&H=16 ADC clks
ADCCTL1 |= ADCSHP | ADCCONSEQ_0 | ADCDIV_2; // ADCCLK = MODOSC; sampling timer
ADCCTL2 |= ADCRES; // 10-bit conversion results
ADCIE |= ADCIE0;
LCD CODE
// Configure LCD pins
SYSCFG2 |= LCDPCTL; // R13/R23/R33/LCDCAP0/LCDCAP1 pins selected
LCDPCTL0 = 0xFFFF;
LCDPCTL1 = 0x07FF;
LCDPCTL2 = 0x00F0; // L0~L26 & L36~L39 pins selected
LCDCTL0 = LCDSSEL_0 | LCDDIV_7; // flcd ref freq is xtclk
// LCD Operation - Mode 3, internal 3.08v, charge pump 256Hz
LCDVCTL = LCDCPEN | LCDREFEN | VLCD_6 | (LCDCPFSEL0 | LCDCPFSEL1 | LCDCPFSEL2 | LCDCPFSEL3);
LCDMEMCTL |= LCDCLRM; // Clear LCD memory
LCDCSSEL0 = 0x000F; // Configure COMs and SEGs
LCDCSSEL1 = 0x0000; // L0, L1, L2, L3: COM pins
LCDCSSEL2 = 0x0000;
LCDM0 = 0x21; // L0 = COM0, L1 = COM1
LCDM1 = 0x84; // L2 = COM2, L3 = COM3
WHILE LOOP - CODE
while(1) {
ADCMCTL0 |= ADCINCH_8 | ADCSREF_0;
ADCCTL0 |= ADCENC | ADCSC ; // Sampling and conversion start
while(ADCCTL1 & ADCBUSY);
sensor[0] = ADCMEM0;
_delay_cycles(10000);
sensor[1]=sensor[0];
for (i = 0 ; i<=3 ; i++ ) {
splitchar[i] |= sensor[1] % 10;
ADCMEM0 = splitchar[i];
sensor[1] |= sensor[1] / 10;
_delay_cycles(10000);
}
LCDMEM[pos6] = digit[(splitchar[0])];
LCDMEM[pos5] = digit[(splitchar[1])];
LCDMEM[pos4] = digit[(splitchar[2])];
LCDMEM[pos3] = digit[(splitchar[3])];
LCDCTL0 |= LCD4MUX | LCDON; // Turn on LCD, 4-mux selected
PMMCTL0_H = PMMPW_H; // Open PMM Registers for write
PMMCTL0_L |= PMMREGOFF_L; // and set PMMREGOFF
}