Other Parts Discussed in Thread: MSP430FR5847, MSP430FR5969
I'm seeing what appear to be several related bugs in Grace 3.0.3.66:
1. I configured to MSP430FR5847 P3DIR and P3OUT, but grace does not initialize for P3 port configurations in PinMux_init.c.
PinMux_init.c:
void PinMux_graceInit(void)
{
/* USER CODE START (section: PinMux_graceInit_prologue) */
/* User initialization code */
/* USER CODE END (section: PinMux_graceInit_prologue) */
/* Port 1 Output Register */
P1OUT = 0;
/* Port 1 Direction Register */
P1DIR = BIT4 | BIT5 | BIT6 | BIT7;
/* Port 1 Interrupt Edge Select */
P1IES = 0;
/* Port 1 Interrupt Flag Register */
P1IFG = 0;
/* Port 2 Output Register */
P2OUT = 0;
/* Port 2 Direction Register */
P2DIR = BIT0 | BIT1 | BIT2 | BIT4 | BIT5 | BIT6 | BIT7;
/* Port 2 Interrupt Edge Select */
P2IES = 0;
/* Port 2 Interrupt Flag Register */
P2IFG = 0;
/* Port J Output Register */
PJOUT = 0;
/* Port J Direction Register */
PJDIR = 0;
/* USER CODE START (section: PinMux_graceInit_epilogue) */
/* User code */
/* USER CODE END (section: PinMux_graceInit_epilogue) */
}
For MSP430FR5969 is OK.
Best Regards,
Yane