This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP432P401R Energy Consumption in LPM3

Hey guys,

I have been struggling the last couple of days trying to evaluate the new msp432 and if it will meet our power requirements for our application.

Basically, I am trying to simply monitor the LPM3 current on the MSP-EXP432P401R launchpad and match it to the msp432's data sheet at expected current consumption in LPM3.

My measurement setup involves programming the board, disconnecting the USB cable, removing all jumpers between the mcu and the on-board emulator, switching the JTAG switch to external debug, and then connecting the positive terminal of a 3.3V battery to the 3V3 pin on J6, while connecting the GND pin on the J6 connector to a 100 ohm resister which in turn is connected to the negative terminal of the battery.  I then use an oscilloscope probe across the resistor to measure the current.

In doing this, I find that once the system enters LPM3, I am measuring roughly 11uA of current, while the msp432 data sheet indicates that we should be around 850 nA (give or take).

Summary of the code is to disable the watchdog, setup the gpio, enable the external 32khz crystal and use it to source BCLK and ACLK.  Then enter LPM3 (so neither RTC nor WTD is enabled).  Possibly I am configuring something wrong?

int main(void)
{

    /* Stop Watchdog  */
	MAP_WDT_A_holdTimer();

	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P1, PIN_ALL8);
	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P2, PIN_ALL8);
	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P3, PIN_ALL8);
	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P4, PIN_ALL8);
	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P5, PIN_ALL8);
	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P6, PIN_ALL8);
	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P7, PIN_ALL8);
	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P8, PIN_ALL8);
	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P9, PIN_ALL8);
	MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P10, PIN_ALL8);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0 | GPIO_PIN2 | GPIO_PIN3 | GPIO_PIN5 | GPIO_PIN6 | GPIO_PIN7);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P2, PIN_ALL8);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P3, PIN_ALL8);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P4, PIN_ALL8);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P5, PIN_ALL8);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P6, PIN_ALL8);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P7, PIN_ALL8);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P8, PIN_ALL8);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P9, PIN_ALL8);
	MAP_GPIO_setAsOutputPin(GPIO_PORT_P10, PIN_ALL8);
	MAP_GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN1 | GPIO_PIN4);
	PJSEL0 = BIT0 | BIT1 | BIT2 | BIT3;
	PJDIR = BIT4 | BIT5;

    CSKEY = 0x695A;                           // Unlock CS module for register access
    CSCTL2 = LFXT_EN;                         // LFXT on
    // Loop until XT1, XT2 & DCO fault flag is cleared
    do
    {
        // Clear XT2,XT1,DCO fault flags
       CSCLRIFG |= CLR_DCORIFG | CLR_HFXTIFG | CLR_LFXTIFG;
       SYSCTL_NMI_CTLSTAT &= ~ SYSCTL_NMI_CTLSTAT_CS_SRC;
    } while (SYSCTL_NMI_CTLSTAT & SYSCTL_NMI_CTLSTAT_CS_FLG);// Test oscillator fault flag
    CSCTL1 = SELS_3 | SELM_3;// Select ACLK as LFXTCLK
    CSKEY = 0;

    while(1)
    {
    	MAP_PCM_gotoLPM3();
    }
}

I appreciate any help anybody can offer!

Thanks,

-Chris

  • I solved my issue.  The problem was due to the High-side supervisor/monitor being in full-performance mode by default.  By eliminating this, I fixed my issue.

  • Chris,

    I'm glad that you were able to find a solution to your problem.  Attached is the recommended code for ideal LPM3 measurements with the MSP432P401R for anyone with a similar question browsing the MSP430 E2E forum.  I will further make sure that we have documentation in place to explain that this is a necessary step for low power measurements.

    Regards,

    Ryan

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2013, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    
    
     *
     *******************************************************************************
    
    
    
    
     *
     *                       MSP432 CODE EXAMPLE DISCLAIMER
    
    
    
    
    
    
    
    
    
     *
     * MSP432 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see http://www.ti.com/tool/mspdriverlib for an API functional
     * library & https://dev.ti.com/pinmux/ for a GUI approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //   MSP432P401 Demo - Enter LPM3 with ACLK = REFO
    //
    //  Description: MSP432 device is configured to enter LPM3 mode with GPIOs properly
    //  terminated. P1.1 is configured as an input. Pressing the button connect to P1.1
    //  results in device waking up and servicing the Port1 ISR. LPM3 current can be
    //  measured when P1.0 is output low (e.g. LED off).
    //
    //  ACLK = 32kHz, MCLK = SMCLK = default DCO
    //
    //
    //               MSP432p401rpz
    //            -----------------
    //        /|\|                 |
    //         | |                 |
    //         --|RST              |
    //     /|\   |                 |
    //      --o--|P1.1         P1.0|-->LED
    //     \|/
    //
    //   Dung Dang
    //   Texas Instruments Inc.
    //   Nov 2013
    //   Built with Code Composer Studio V6.0
    //******************************************************************************
    
    
    
    #include "msp.h"
    int main(void)
    {
    
    
    
        /* Hold the watchdog */
        WDTCTL = WDTPW | WDTHOLD;
        /* Configuring P1.0 as output and P1.1 (switch) as input with pull-up resistor*/
        /* Rest of pins are configured as output low */
        /* Notice intentional '=' assignment since all P1 pins are being deliberately configured */
        P1DIR = ~(BIT1);
        P1OUT = BIT1;
        P1REN = BIT1;                           // Enable pull-up resistor (P1.1 output high)
        P1SEL0 = 0;
        P1SEL1 = 0;
        P1IFG = 0;                              // Clear all P1 interrupt flags
        P1IE = BIT1;                            // Enable interrupt for P1.1
        P1IES = BIT1;                               // Interrupt on high-to-low transition
    
        // Enable Port 1 interrupt on the NVIC
        NVIC_ISER1 = 1 << ((INT_PORT1 - 16) & 31);
    
        // Terminate all remaining pins on the device
        P2DIR |= 0xFF; P2OUT = 0;
        P3DIR |= 0xFF; P3OUT = 0;
        P4DIR |= 0xFF; P4OUT = 0;
        P5DIR |= 0xFF; P5OUT = 0;
        P6DIR |= 0xFF; P6OUT = 0;
        P7DIR |= 0xFF; P7OUT = 0;
        P8DIR |= 0xFF; P8OUT = 0;
        P9DIR |= 0xFF; P9OUT = 0;
        P10DIR |= 0xFF; P10OUT = 0;
    
        /* Configure Port J */
        PJDIR |= (BIT2 | BIT3); PJOUT &= ~(BIT2 | BIT3);
    
        /* PJ.0 & PJ.1 configured for XT1 */
        PJSEL0 |= BIT0 | BIT1;
        PJSEL1 &= ~(BIT0 | BIT1);
    
        /* Starting LFXT in non-bypass mode without a timeout. */
        CSKEY = CSKEY_VAL;
        CSCTL1 &= ~(SELA_M | SELB);
        CSCTL1 |= SELA__LFXTCLK;                // Source LFXTCLK to ACLK & BCLK
        CSCTL2 &= ~(LFXTDRIVE_M);               // Configure to lowest drive-strength
    
        CSCTL2 |= LFXT_EN;
        while (CSIFG & LFXTIFG)
            CSCLRIFG |= LFXTIFG;
        CSKEY = 0;
    
        /* Turn off PSS high-side & low-side supervisors */
        PSSKEY = PSS_KEY_KEY_VAL;
        PSSCTL0 |= SVSMHOFF | SVSLOFF;
        PSSKEY = 0;
    
        /* Enable PCM rude mode, which allows to device to enter LPM3 without waiting for peripherals */
        PCMCTL1 = PCM_CTL_KEY_VAL | FORCE_LPM_ENTRY;
    
    
        /* Enable all SRAM bank retentions prior to going to LPM3  */
        SYSCTL_SRAM_BANKRET |= SYSCTL_SRAM_BANKRET_BNK7_RET;
        __enable_interrupt();
        SCB_SCR |= SCB_SCR_SLEEPONEXIT;        // Do not wake up on exit from ISR
    
    while(1)
    {
        /* Setting the sleep deep bit */
        SCB_SCR |= (SCB_SCR_SLEEPDEEP);
        /* Go to LPM3 */
        __sleep();
    }
    }
    
    /* Port1 ISR */
    void Port1Handler(void)
    {
        volatile uint32_t i, status;
        /* Toggling the output on the LED */
        if(P1IFG & BIT1)
            P1OUT ^= BIT0;
    
        /* Delay for switch debounce */
        for(i = 0; i < 10000; i++)
    
        P1IFG &= ~BIT1;
    
    }
    

**Attention** This is a public forum