Other Parts Discussed in Thread: MSP430FR5969, ENERGIA
I would like to generate a PWM on P1.2 or P1.3 or P1.4 since these pins can be connected to a wire ...There is software example for P1.0 and P1.1 which are LEDs which is the following...
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
// Configure GPIO
P1DIR |= BIT0 | BIT1; // P1.0 and P1.1 output
P1SEL0 |= BIT0 | BIT1; // P1.0 and P1.1 options select
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
CSCTL0_H = CSKEY >> 8; // Unlock CS registers
CSCTL1 = DCOFSEL_6; // Set DCO = 8MHz
CSCTL2 = SELA__VLOCLK | SELS__DCOCLK | SELM__DCOCLK;// Set ACLK=VLO SMCLK=DCO
CSCTL3 = DIVA__8 | DIVS__8 | DIVM__8; // Set all dividers
CSCTL0_H = 0; // Lock CS registers
// Configure Timer0_A
TA0CCR0 = 1000-1; // PWM Period
TA0CCTL1 = OUTMOD_7; // CCR1 reset/set
TA0CCR1 = 750; // CCR1 PWM duty cycle
TA0CCTL2 = OUTMOD_7; // CCR2 reset/set
TA0CCR2 = 250; // CCR2 PWM duty cycle
TA0CTL = TASSEL__SMCLK | MC__UP | TACLR; // SMCLK, up mode, clear TAR
__bis_SR_register(LPM0_bits); // Enter LPM0
__no_operation(); // For debugger
}
when i try change P1DIR |= BIT0 | BIT1; // P1.0 and P1.1 output
P1SEL0 |= BIT0 | BIT1;
to
P1DIR |= BIT0 | BIT2; // P1.0 and P1.2output
P1SEL0 |= BIT0 | BIT2;
i dont get any output for p1.2?...please tell me how to scale the same program for p1.2 and other p1.x pins...