I recently bought TI's MSP-FET430UIF Evaluation Board/Kit with the CCSv4.0 software but was unable to get it to communicate with my target. The target board is very simple, apart from an MSP430F2013 (14-pin DIP) its only other components are a 3V regulator and a 100 kOhm/1 nF reset circuit. After searching the web for a solution I looked at my computer's Device Manager and found "Texas Instruments XDS560 PCI JTAG Emulator" with an exclamation point ! There were no entries under "Universal Serial Bus controllers". At a loss for what to do I recently (22-Apr) downloaded and installed ccsv4.1 onto my computer and tried again to get the debugger to communicate with the MSP430F2013 via the 4-wire JTAG pins. All I can get is the same old message - "Error connecting to target: No MSP430 device was found on USB FET 1".
Can anybody tell me:
Why is there a reference to XDS560 in the Device Manager? Under properties it says only "This device cannot start. (code 10)"
Why is there no entry in the Device Manager's USB Controller section? Surely there should be one.
How can I be sure my debugger is working in 4-wire JTAG mode and not 2-wire JTAG Spy-Bi-Wire mode? Where is this set in CCSv4.1?
Why won't it work?
Thanks.