This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CCS 6 cannot connect to target AFE4403 EVM , USB0,1,2 all fail, UART either. MSP-FET430UIF Jtag Emulator talk normally the target AFE4403 EVM.
I do not know what is wrong in CCS6 which is free license. Do I have to purchase regular Licensed CCS software to attach the target automatically& properly ?
============ Below is detection error ( AFE4403EVM COM port is 20 , not 65. I do not know where 65 comes from . )
MSP430: Trouble Writing Memory Block at 0x4400 on Page 0 of Length 0x3ee2: **Error**: Serial Communication failed at port: COM65, baud rate:9600! To use serial monitor, please ensure the following prerequisites are satisfied: 1. Make sure the cable is plugged into both the target and the host on the right COM port. 2. Make sure a compatible target side serial monitor is loaded and running on the target device.
MSP430: File Loader: Verification failed: Target failed to write 0x4400
MSP430: GEL: File: D:\WristWatchFW\CES_HRMWatch_PC_EVM_GUI_v2.0-CCS\Debug\CES_HRMWatch_PC_EVM_GUI_v2.0-CCS.out: Load failed.
Look forward to clear clue !!
430UIF Jtag Emulator program normally EVM, problem is at CCS 6.1 . Why CCS look for COM65 ? Send me URL, good CCS setting documents .
Stanley,
Here is a URL for all the documentation on CCS.
http://www.ti.com/tool/ccstudio?dcmp=PPC_Google_TI&k_clickid=219a9259-d74c-403b-b869-db500ecff4c1#Technical%20Documents