This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 Specific PWM Signal

Please I do need Help !! ><
PLEASE HELP ME

i am using MSP430 2533.

1. I need to produce two PWM wave form at the same time, both with 25% Duty Cycle and with one shifted 180 phase from the other.
Here are the wave forms ><


Firsttttt: |-|___|-|___|-|___|-|_
Second: __|-|___|-|___|-|___

each with 25% Duty Cycle
><

2. And both of the two have to be output in 1.8V (How can i set the voltage ><)QQ
Please do help me

**Attention** This is a public forum