This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't seem to new-up an object

Other Parts Discussed in Thread: CCSTUDIO, MSP430G2210, MSP-FET

Folks,

This is my first foray into CCStudio.  Until now, I was writing in C for microcontrollers and in C# for Windows.  I also have some past training in C++ for PC.  So, I'm not entirely new to this.  But unfortunately, I'm stuck.

I have declared two classes I2CBusBase and its child I2CBusViaBitBanging.  The code compiles.  But when I try to new-up the object,

I2CBusBase* pI2CBus = new I2CBusViaBitBanging();

The object is not created, and the pI2CBus points to 0x0000.  On the other hand, if I do

I2CBusViaBitBanging theBus;

The object is created as expected, and it behaves as expected.  This suggests that the constructors in the classes should function okay.

I must be missing something.  Any suggestion, insight or reference is really appreciated!

Cheers,
- Nick

My development environment: CCStudio 6.1.0.00104, MSP-FET via Spy-Bi-Wire, MSP430G2210.  I can post more code if needed, of course.

**Attention** This is a public forum