The datasheet says 0.1uF but the EXP430FR4133 Launchpad Schematic shows a 1.0uF cap on that pin. In both cases, a 0.1uF cap is specified for the three LCD resistor I/O pins
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The datasheet says 0.1uF but the EXP430FR4133 Launchpad Schematic shows a 1.0uF cap on that pin. In both cases, a 0.1uF cap is specified for the three LCD resistor I/O pins
After talking to the team that designed the Launchpad, it sounds like they experimented with a few different size capacitors with the particular display used on the Launchpad, and found that the larger capacitor helped them to achieve better contrast with this particular LCD glass. If you already have a particular LCD in mind, it might be a good idea to wire it up and do some of your own tests with different values to try to see what gives you the best result (with a minimum of 0.1uF). This kind of testing is a good thing to do for an LCD design anyway, because LCDs can need a lot of fine-tuning depending on the display to get the desired contrast/appearance that you are looking for - it would let you experiment with other things as well (such as whether you can use the internal bias caps or need to use external ones) before locking in on a final design. You can find more information on different things that affect contrast and LCD appearance in the app note www.ti.com/lit/pdf/slaa654
Regards,
Katie
I just noticed that the LCD_E section of the Famly Guide does address this question on page 385: "When the internal charge pump is used, a 100-nF or larger capacitor must be connected between the LCDCAP0 and LCDCAP1 pins."
Hi, Katie and Nick,
Yes, 0.1uF or larger capacitor should be for LCDCAP0 and LCDCAP1 pins.
The selection guide for the capacitor value: 0.1uF can get lowest power consumption for LCD_E. But with low charge pump frequency, the 0.1uF may result in LCD contrast not very good. For this case, increasing the capacitor value can help. So it is a tradeoff between LCD contrast and low power consumption for LCD. You can select appropriate capacitro value based on the charge pump frequency setting, LCD contrast and the power consumption requirement.
Best Regards,
Lixin
**Attention** This is a public forum