This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 7
Views: 2869
Just installed Code Composer Studio Version: 6.1.1.00022 on Window 7 64 bit systems.
When trying to load any example project using TI Resource Explorer I get
CreateProcess error=267 directroy name is invalid.
No old versions have been installed first time for CCS on system. Tried another computer with same results?
I see the same error with my installation of CCS 6.1.1 and MSPWare version 2.30.00.49. I will move this to the MSP430 forum for the MSPWare experts to take a look.
____________________________________________________________________________
Please click This Resolved My Issue if the reply answers your question.
Explore Code Composer Studio documentation and resources using online Resource ExplorerTrack a known bug with SDOWP. Enter the bug id in the "Find Record ID" box
I ran into the same error yesterday. It's been reported.
I found two workarounds:
Hope this helps,Scott
Charles,
Seems to be an incompatibility between MSPWare 2.30.00 and CCS 6.1.1. If you don't need any of the features of CCS 6.1.1 you can install CCS 6.1.0 until we have worked out the fix.
Thanks for the bug report,Zack
----------------------------------------------------------------------------------------------------------------Please click the Verify Answer button on this post if it answers your question.----------------------------------------------------------------------------------------------------------------
In reply to Zack L.:
In reply to Raged:
RagedCan CCS 6.1.1 and CCS 6.1.0 coexist? (i.e. does installing one wipe the other?)
Yes they can co-exist as long as they are installed to different folders.
In reply to AartiG:
AartiG Raged Can CCS 6.1.1 and CCS 6.1.0 coexist? (i.e. does installing one wipe the other?) Yes they can co-exist as long as they are installed to different folders.
Raged Can CCS 6.1.1 and CCS 6.1.0 coexist? (i.e. does installing one wipe the other?)
Thank you!
Are you sure that the problem is in CSS v6.1.1...?
I have the same problem but have the impression that this was created after upgrading MSPWare.
The older version of ‘MSP430ware’ can I use without problems with v6.1.1....